<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: ISP over SPI</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-SPI/m-p/902277#M36213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="341746" data-username="tdenis8" href="https://community.nxp.com/people/tdenis8"&gt;Tomislav Denis&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is there any special command that I need to use when reading the response? Or I simply have to read response(from the previous command) when executing the next command?&lt;BR /&gt;-- The host will receive the response from the MCU after sending the command&lt;BR /&gt;2) Is there any ISP over SPI host tool(example)?&lt;BR /&gt;-- I'm afraid there's no similar tool as you want.&lt;BR /&gt;3) Better documentation on this topic than LPC546xx User manual?&lt;BR /&gt;-- No, I'm afraid not.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 May 2019 02:31:00 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2019-05-22T02:31:00Z</dc:date>
    <item>
      <title>ISP over SPI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-SPI/m-p/902276#M36212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using a LPC5418 (OM13094 demo board).&lt;/P&gt;&lt;P&gt;I am trying to do ISP over SPI and after sending appropriate SPI command I would like to read response!&lt;/P&gt;&lt;P&gt;My first try was to simply read response by writing appropriate number of 0x00 to LPC and shifting out response. This works but I have problem that ISP command handler tries to decode those 0x00 and interprets them as new command! So at the end when executing next command I am getting response INVALID_COMMAND (0x55 0x00 0x04 0x00 0x01).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My quations are:&lt;BR /&gt;- Is there any special command that I need to use when reading response? Or I simply have to read response(from previous command) when executing next command?&lt;BR /&gt;- Is there any ISP over SPI host tool(example)?&lt;BR /&gt;- Better documentation on this topic than LPC546xx User manual?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2019 11:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-SPI/m-p/902276#M36212</guid>
      <dc:creator>tdenis8</dc:creator>
      <dc:date>2019-05-21T11:10:35Z</dc:date>
    </item>
    <item>
      <title>Re: ISP over SPI</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-SPI/m-p/902277#M36213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="341746" data-username="tdenis8" href="https://community.nxp.com/people/tdenis8"&gt;Tomislav Denis&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is there any special command that I need to use when reading the response? Or I simply have to read response(from the previous command) when executing the next command?&lt;BR /&gt;-- The host will receive the response from the MCU after sending the command&lt;BR /&gt;2) Is there any ISP over SPI host tool(example)?&lt;BR /&gt;-- I'm afraid there's no similar tool as you want.&lt;BR /&gt;3) Better documentation on this topic than LPC546xx User manual?&lt;BR /&gt;-- No, I'm afraid not.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 02:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-SPI/m-p/902277#M36213</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-05-22T02:31:00Z</dc:date>
    </item>
  </channel>
</rss>