<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1788 Ethernet</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Ethernet/m-p/901532#M36199</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rafael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order for you to get the best support regarding the behavior you are experiencing, I highly recommend contacting the ARM support team directly, because you are using the CMSIS libraries for ethernet.&lt;/P&gt;&lt;P&gt;Also, I would recommend checking the ethernet examples provided in the LPCOpen, if you would like extra references. However, these examples don't use the CMSIS libraries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you would like more information do let me know.&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 May 2019 16:42:07 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2019-05-22T16:42:07Z</dc:date>
    <item>
      <title>LPC1788 Ethernet</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Ethernet/m-p/901531#M36198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm facing a problem with the Ethernet interface of the LPC1788 microcontroller. Sometimes, after a time operating normally, the ping reply time suddenly gets higher. When this happens, there is no way to&amp;nbsp;recover the interface from this behavior (just turning the board off and on again). I saw already (debugging the system) that when ping response times gets higher, the RX Consume index is different from the RX Produce index, unlike the normal operation, where the 2 indexes (Produce and Consume) are always equal.&amp;nbsp;I'm using CMSIS driver for the Ethernet peripheral.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone ever experienced this? Any idea of what it could be?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 17:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Ethernet/m-p/901531#M36198</guid>
      <dc:creator>rafaelzingler</dc:creator>
      <dc:date>2019-05-20T17:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 Ethernet</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Ethernet/m-p/901532#M36199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rafael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order for you to get the best support regarding the behavior you are experiencing, I highly recommend contacting the ARM support team directly, because you are using the CMSIS libraries for ethernet.&lt;/P&gt;&lt;P&gt;Also, I would recommend checking the ethernet examples provided in the LPCOpen, if you would like extra references. However, these examples don't use the CMSIS libraries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you would like more information do let me know.&lt;/P&gt;&lt;P&gt;Have a great day!&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 16:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-Ethernet/m-p/901532#M36199</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-05-22T16:42:07Z</dc:date>
    </item>
  </channel>
</rss>