<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Problem caused by a difference between two demo board revision ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899135#M36102</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use a LPCXpresso546xx/540xx revision E and for the test, I use the emc_sdram program from SDK_2.5.0_LPCXpresso54628.&lt;BR /&gt;Yesterday, I modified the specific time "SDRAM_TRP_NS" in the file "board.c" with the other specific times with the values given in the datasheet from Winbond. The error is again present but when I modify the SDRAM_TRP_NS value with higher value than value in datasheet, there is not error left.&lt;BR /&gt;Other interesting fact : when I set the frequency of the EMC bus to 110 MHz (after setting the AHB bus' clock to 220 MHz), the value given in datasheet (for SDRAM_TRP_NS) doesn't cause error anymore.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Apr 2019 08:05:43 GMT</pubDate>
    <dc:creator>benjamin3</dc:creator>
    <dc:date>2019-04-18T08:05:43Z</dc:date>
    <item>
      <title>Problem caused by a difference between two demo board revision ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899133#M36100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have a problem with the code example from a SDK from NXP about the EMC bus to use an external SDRAM. I use the LPCXpresso 546xx/540xx demo board from NXP.&lt;/P&gt;&lt;P&gt;The code example works correctly when I use the demo board LPCxpresso546xx/540xx with an external SDRAM from Micron ( &lt;SPAN class=""&gt;MT48LC8M16A2B4&lt;/SPAN&gt;) but when I use the demo board LPCxpresso546xx/540xx with an external SDRAM from Winbond (&lt;SPAN class=""&gt;W9812G6JB-6I&lt;/SPAN&gt;), the program says that there is an error when it checks the written data in the external SDRAM memory.&lt;/P&gt;&lt;P&gt;I was able to see in the memory that there is an error during data writing step :&lt;/P&gt;&lt;P&gt;Normally, the program writes (from the 0xA0000000 address) data from 0 and increasing each value by 1 compared with the previous value (ex : 00000000, 00000001, ...., 0000000A, 0000000B). However, at an address the written value is not correct compared with the others (ex : 000002FC, 000002FD, 000002FE, &lt;EM&gt;&lt;STRONG&gt;6B836021&lt;/STRONG&gt;&lt;/EM&gt;, 00000300, 00000301, the wrong value is at the address 0xa0000bfc but at each try, the address with the wrong value is not the same).&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Benjamin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 10:07:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899133#M36100</guid>
      <dc:creator>benjamin3</dc:creator>
      <dc:date>2019-04-17T10:07:50Z</dc:date>
    </item>
    <item>
      <title>Re: Problem caused by a difference between two demo board revision ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899134#M36101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="339898" data-username="benjamin@lightingsoft.com" href="https://community.nxp.com/people/benjamin@lightingsoft.com"&gt;Benjamin Hainaut&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;Before answering the question, I was wondering if you can introduce the condition and steps of replicating the phenomenon, for instance, the demo boards, demo code, etc, as it will help me to figure it out.&lt;BR /&gt;Looking forward to your reply.&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 01:41:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899134#M36101</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-04-18T01:41:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem caused by a difference between two demo board revision ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899135#M36102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use a LPCXpresso546xx/540xx revision E and for the test, I use the emc_sdram program from SDK_2.5.0_LPCXpresso54628.&lt;BR /&gt;Yesterday, I modified the specific time "SDRAM_TRP_NS" in the file "board.c" with the other specific times with the values given in the datasheet from Winbond. The error is again present but when I modify the SDRAM_TRP_NS value with higher value than value in datasheet, there is not error left.&lt;BR /&gt;Other interesting fact : when I set the frequency of the EMC bus to 110 MHz (after setting the AHB bus' clock to 220 MHz), the value given in datasheet (for SDRAM_TRP_NS) doesn't cause error anymore.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 08:05:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899135#M36102</guid>
      <dc:creator>benjamin3</dc:creator>
      <dc:date>2019-04-18T08:05:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problem caused by a difference between two demo board revision ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899136#M36103</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="339898" data-username="benjamin@lightingsoft.com" href="https://community.nxp.com/people/benjamin@lightingsoft.com" rel="noopener noreferrer" target="_blank"&gt;Benjamin Hainaut,&lt;/A&gt; &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thanks for your reply.&lt;BR /&gt;I only have one rev E board on hand, it's LPCXpresso54018.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.jpg"&gt;&lt;IMG alt="pastedImage_1.jpg" src="https://community.nxp.com/t5/image/serverpage/image-id/65352i7A056944B7DDD29C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.jpg" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;It doesn't encounter a similar error as you mentioned above when running the emc_sdram code.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;IMG alt="pastedImage_2.png" src="https://community.nxp.com/t5/image/serverpage/image-id/66320i3FC6EEE346CBE124/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" /&gt;&lt;/SPAN&gt;&lt;BR /&gt;I've also attached the BOARD_InitSDRAM() function below, please check it.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#ifdef W9812G6JB6I&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_REFRESHPERIOD_NS (64 * 1000000 / 4096) &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;/* 4096 rows/ 64ms */&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_TRP_NS (20u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_TRAS_NS (42u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_TSREX_NS (72u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_TAPR_NS (18u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_TWRDELT_NS (12u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_TRC_NS (60u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_RFC_NS (60u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_XSR_NS (67u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_RRD_NS (12u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_MRD_NCLK (2u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_RAS_NCLK (2u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_MODEREG_VALUE (0x23u)&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#define SDRAM_DEV_MEMORYMAP (0x09u) &lt;/SPAN&gt;&lt;SPAN class="comment token"&gt;/* 128Mbits (8M*16, 4banks, 12 rows, 9 columns)*/&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#endif&lt;/SPAN&gt;

&lt;SPAN class="comment token"&gt;/* Initialize the external memory. */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;BOARD_InitSDRAM&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
    emc_basic_config_t basicConfig&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    emc_dynamic_timing_config_t dynTiming&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    emc_dynamic_chip_config_t dynChipConfig&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    &lt;SPAN class="comment token"&gt;/* Basic configuration. */&lt;/SPAN&gt;
    basicConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;endian &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kEMC_LittleEndian&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    basicConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;fbClkSrc &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kEMC_IntloopbackEmcclk&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="comment token"&gt;/* EMC Clock = CPU FREQ/2 here can fit CPU freq from 12M ~ 180M.
     * If you change the divide to 0 and EMC clock is larger than 100M
     * please take refer to emc.dox to adjust EMC clock delay.
     */&lt;/SPAN&gt;
    basicConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;emcClkDiv &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="comment token"&gt;/* Dynamic memory timing configuration. */&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;readConfig &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kEMC_Cmddelay&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;refreshPeriod_Nanosec &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_REFRESHPERIOD_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tRp_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_TRP_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tRas_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_TRAS_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tSrex_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_TSREX_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tApr_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_TAPR_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tWr_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1000000000&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;/&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;CLOCK_GetFreq&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;kCLOCK_EMC&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt; SDRAM_TWRDELT_NS&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;/* one clk + 6ns */&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tDal_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tWr_Ns &lt;SPAN class="operator token"&gt;+&lt;/SPAN&gt; dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tRp_Ns&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tRc_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_TRC_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tRfc_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_RFC_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tXsr_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_XSR_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tRrd_Ns &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_RRD_NS&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynTiming&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;tMrd_Nclk &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_MRD_NCLK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="comment token"&gt;/* Dynamic memory chip specific configuration: Chip 0 - W9812G6JB-6I */&lt;/SPAN&gt;
    dynChipConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;chipIndex &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynChipConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;dynamicDevice &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; kEMC_Sdram&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynChipConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;rAS_Nclk &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_RAS_NCLK&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynChipConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sdramModeReg &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_MODEREG_VALUE&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    dynChipConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sdramExtModeReg &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;/* it has no use for normal sdram */&lt;/SPAN&gt;
    dynChipConfig&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;devAddrMap &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; SDRAM_DEV_MEMORYMAP&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="comment token"&gt;/* EMC Basic configuration. */&lt;/SPAN&gt;
    &lt;SPAN class="token function"&gt;EMC_Init&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;EMC&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;basicConfig&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="comment token"&gt;/* EMC Dynamc memory configuration. */&lt;/SPAN&gt;
    &lt;SPAN class="token function"&gt;EMC_DynamicMemInit&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;EMC&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;dynTiming&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;dynChipConfig&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Nov 2020 14:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899136#M36103</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2020-11-02T14:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Problem caused by a difference between two demo board revision ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899137#M36104</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer, it works correctly.&lt;/P&gt;&lt;P&gt;The problem went from a wrong setting of the specific times (&lt;CODE&gt;&lt;SPAN class=""&gt;SDRAM_TRP_NS, SDRAM_TRAS_NS ect ...).&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Benjamin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 15:41:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-caused-by-a-difference-between-two-demo-board-revision/m-p/899137#M36104</guid>
      <dc:creator>benjamin3</dc:creator>
      <dc:date>2019-04-19T15:41:23Z</dc:date>
    </item>
  </channel>
</rss>