<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPCXpresso54608 emWin support 10 inch LCD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608-emWin-support-10-inch-LCD/m-p/897469#M36024</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPCXpresso54608 emWin is equipped with 4.3" LCD. If the LCD is changed to 8"~10" LCD,&lt;/P&gt;&lt;P&gt;then the emWin library can still support such a LCD without version updated/?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 May 2019 17:17:36 GMT</pubDate>
    <dc:creator>gary12kuo</dc:creator>
    <dc:date>2019-05-16T17:17:36Z</dc:date>
    <item>
      <title>LPCXpresso54608 emWin support 10 inch LCD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608-emWin-support-10-inch-LCD/m-p/897469#M36024</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPCXpresso54608 emWin is equipped with 4.3" LCD. If the LCD is changed to 8"~10" LCD,&lt;/P&gt;&lt;P&gt;then the emWin library can still support such a LCD without version updated/?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 May 2019 17:17:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608-emWin-support-10-inch-LCD/m-p/897469#M36024</guid>
      <dc:creator>gary12kuo</dc:creator>
      <dc:date>2019-05-16T17:17:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso54608 emWin support 10 inch LCD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608-emWin-support-10-inch-LCD/m-p/897470#M36025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gary,&lt;/P&gt;&lt;P&gt;emWin is Segger product, and it is supported by Segger. Please contact Segger for it.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://www.segger.com/emwin.html" title="http://www.segger.com/emwin.html"&gt;emWin - The Embedded GUI by SEGGER | It simply works!&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2019 06:15:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCXpresso54608-emWin-support-10-inch-LCD/m-p/897470#M36025</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-05-20T06:15:09Z</dc:date>
    </item>
  </channel>
</rss>