<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC84x FlashROM Data retention in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892267#M35774</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean with ROM type NOR, the internal structure? if this is the case this information can not be shared, this is internal information&lt;/P&gt;&lt;P&gt;On the following link, you can see some information about how the data retention is calculated, this is a reference&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/engineering-bulletin/EB618.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB618.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And yes with more temperature range there are more probabilities of failures, but there is not a formula that can be shared&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Jun 2019 15:49:04 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2019-06-11T15:49:04Z</dc:date>
    <item>
      <title>LPC84x FlashROM Data retention</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892266#M35773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Is the flash ROM of the LPC84x NOR type?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;2. Does this data retention period mean the life is calculated from the number of read errors that occur as a result of accelerated testing with the temperature turned on with the power on?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;3. I think that the probability that the error of the flash ROM occurs in the power ON state changes with the temperature condition, for example, when the standard of Tamb = -40 ° C to +105 ° C is relaxed from -20 ° C to +70 ° C etc., the period is extended Is it?&lt;BR /&gt;I would be happy if you could tell me the formula.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# I do not think that English is not good.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2019 04:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892266#M35773</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-05-14T04:55:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC84x FlashROM Data retention</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892267#M35774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean with ROM type NOR, the internal structure? if this is the case this information can not be shared, this is internal information&lt;/P&gt;&lt;P&gt;On the following link, you can see some information about how the data retention is calculated, this is a reference&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/engineering-bulletin/EB618.pdf"&gt;https://www.nxp.com/docs/en/engineering-bulletin/EB618.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And yes with more temperature range there are more probabilities of failures, but there is not a formula that can be shared&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 15:49:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892267#M35774</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2019-06-11T15:49:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC84x FlashROM Data retention</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892268#M35775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was able to understand the data retention characteristics.&lt;/P&gt;&lt;P&gt;I asked because the LPC series was MIN 10 years.&lt;/P&gt;&lt;P&gt;I understand this matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 23:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC84x-FlashROM-Data-retention/m-p/892268#M35775</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-06-11T23:49:39Z</dc:date>
    </item>
  </channel>
</rss>