<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can the currently used flash bank be determined? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891747#M35748</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i want to write data of a new software-image&amp;nbsp;via IAP (In Application Programming) to this one of flash-banks (A and B), which is&amp;nbsp;currently&amp;nbsp;NOT&amp;nbsp;in use to not run into conflict with parts of the&amp;nbsp;running application located on the currently used flash-bank.&lt;/P&gt;&lt;P&gt;Within the user-manual of LPC43xx&amp;nbsp;i only found&amp;nbsp;the&amp;nbsp;command "Chip_IAP_SetBootFlashBank(..)" for setting the boot&amp;nbsp;flash-bank to A or B.&lt;/P&gt;&lt;P&gt;But what I need is to evaluate the used flash-bank (e.g. A) in the first place and set the boot flash-bank (B) in the second place.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 May 2019 09:26:05 GMT</pubDate>
    <dc:creator>mario_goeckel_e</dc:creator>
    <dc:date>2019-05-13T09:26:05Z</dc:date>
    <item>
      <title>Can the currently used flash bank be determined?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891747#M35748</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i want to write data of a new software-image&amp;nbsp;via IAP (In Application Programming) to this one of flash-banks (A and B), which is&amp;nbsp;currently&amp;nbsp;NOT&amp;nbsp;in use to not run into conflict with parts of the&amp;nbsp;running application located on the currently used flash-bank.&lt;/P&gt;&lt;P&gt;Within the user-manual of LPC43xx&amp;nbsp;i only found&amp;nbsp;the&amp;nbsp;command "Chip_IAP_SetBootFlashBank(..)" for setting the boot&amp;nbsp;flash-bank to A or B.&lt;/P&gt;&lt;P&gt;But what I need is to evaluate the used flash-bank (e.g. A) in the first place and set the boot flash-bank (B) in the second place.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 09:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891747#M35748</guid>
      <dc:creator>mario_goeckel_e</dc:creator>
      <dc:date>2019-05-13T09:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can the currently used flash bank be determined?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891748#M35749</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="326541" data-username="mario.goeckel.ext@siemens-healthineers.com" href="https://community.nxp.com/people/mario.goeckel.ext@siemens-healthineers.com"&gt;Mario Göckel,&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;To be honest, I'm a bit confused with the mean of 'what I need is to evaluate the used flash-bank (e.g. A) in the first place'.&lt;BR /&gt;Whether you want an indicator to tell which flash bank is active now, please explain it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2019 02:14:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891748#M35749</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-05-14T02:14:55Z</dc:date>
    </item>
    <item>
      <title>Re: Can the currently used flash bank be determined?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891749#M35750</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello and thanks for the fast response,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, i need an indicator, which tells me which flash bank is active.&lt;/P&gt;&lt;P&gt;Here i already found FLASHCFGA, FLASHCFGB and i am reading bit31 of these registers.&lt;/P&gt;&lt;P&gt;Of cource i could have written a function and a function pointer, pointing to this function and just reading this address to know which flash bank is used, but this would only be a workaround.&lt;/P&gt;&lt;P&gt;I guess this issue can be closed now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mario Göckel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Von: jeremyzhou &lt;/P&gt;&lt;P&gt;Gesendet: Dienstag, 14. Mai 2019 04:16&lt;/P&gt;&lt;P&gt;An: Goeckel, Mario (ext) (SHS PV R&amp;amp;D-PE MDGC)&lt;/P&gt;&lt;P&gt;Betreff: You have been mentioned by jeremyzhou in Re: Can the currently used flash bank be determined? in NXP Community&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You have been mentioned&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;by jeremyzhou&amp;lt;https://community.nxp.com/people/jeremyzhou?et=notification.mention&amp;gt; in Re: Can the currently used flash bank be determined? in NXP Community - View jeremyzhou's reference to you&amp;lt;https://community.nxp.com/message/1150794?commentID=1150794&amp;amp;et=notification.mention#comment-1150794&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 May 2019 06:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-currently-used-flash-bank-be-determined/m-p/891749#M35750</guid>
      <dc:creator>mario_goeckel_e</dc:creator>
      <dc:date>2019-05-14T06:02:44Z</dc:date>
    </item>
  </channel>
</rss>