<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Error when reselect debugging</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891746#M35747</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Debug Probe Driver for Linux is not necessary/possible, I think. I replaced the firmware with dd if=....., but the problem is still there. Another Linux is no option for that reason.&lt;/P&gt;&lt;P&gt;So I fitted JP2 and attached my J-Link EDU. The problem disappeared, it's much much faster and I'm happy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Apr 2019 09:50:20 GMT</pubDate>
    <dc:creator>1234567890</dc:creator>
    <dc:date>2019-04-19T09:50:20Z</dc:date>
    <item>
      <title>Error when reselect debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891742#M35743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same error on 2 different machines (both Kubuntu 18.04 64 bit, MCUXPresso 10.3.1 and SDK for LPC845 Version 2.5.0:&lt;/P&gt;&lt;P&gt;I abort debugging by clicking the red symbol in the upper menu. Then (doing some other things or even not) I click "Debug" in the Quickstart Panel. Then these windows appear on each other (the right one on top):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79764iC8D302DE4CE84671/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The window in the middle has these "Details":&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79765iF6F8A0E3422DAAD1/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Then I have to click "Escape" a few times until all windows have disappeared. Then I can click "Debug" again and it works. Every time.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2019 19:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891742#M35743</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2019-04-10T19:21:53Z</dc:date>
    </item>
    <item>
      <title>Re: Error when reselect debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891743#M35744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;Whether you can use some screenshots to introduce the complete debug process.&lt;BR /&gt;In further, I was wondering if you try to unplug the board, then plug again, before clicking the debug icon. If not, please give a try.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2019 02:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891743#M35744</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-04-12T02:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error when reselect debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891744#M35745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;unplugging the board everytime works, but can't be the solution. The problem occurs every time I quit a debug session by clicking the icon at the top (red rectangle in the middle):&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62206i80CDE85AD0E313A4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Apr 2019 15:45:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891744#M35745</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2019-04-16T15:45:44Z</dc:date>
    </item>
    <item>
      <title>Re: Error when reselect debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891745#M35746</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;BR /&gt;Firstly, I'd like to suggest you reinstall the NXP LPC11Uxx Debug Probe Driver and firmware ( Attachment is the package of firmware and Windows drivers for LPCXpresso boards with an LPC11U35 debug probe.), then try to debug the LPC845 board again.&lt;BR /&gt;In addition, whether you encounter the same phenomenon when you use another Linux OS, likes Ubuntu.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2019 03:01:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891745#M35746</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-04-17T03:01:34Z</dc:date>
    </item>
    <item>
      <title>Re: Error when reselect debugging</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891746#M35747</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Debug Probe Driver for Linux is not necessary/possible, I think. I replaced the firmware with dd if=....., but the problem is still there. Another Linux is no option for that reason.&lt;/P&gt;&lt;P&gt;So I fitted JP2 and attached my J-Link EDU. The problem disappeared, it's much much faster and I'm happy.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Apr 2019 09:50:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Error-when-reselect-debugging/m-p/891746#M35747</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2019-04-19T09:50:20Z</dc:date>
    </item>
  </channel>
</rss>