<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC Channels in LPC54608J512BD208 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Channels-in-LPC54608J512BD208/m-p/890162#M35688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prasanna,&lt;/P&gt;&lt;P&gt;Regarding your question, as far as I know the LPC546xx only supports SWD mode for downloading/debugging code, the JTAG port is ONLY used for JTAG&amp;nbsp; boundary scan function, in other words, you can not use JTAG port to download code and debugging.&lt;/P&gt;&lt;P&gt;I have seen that the SWD signals are multiplexed with ADC0 pins for LPC546xx, I think you can use a jumper to solve the issue, in development stage, you can connect the SWD pins to a connector, while you can use a jumper to connect the SWD pins to ADC analog source. After development phase, you can close the jump, in this way, the SWD pins are ADC pins.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 May 2019 07:08:05 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-05-13T07:08:05Z</dc:date>
    <item>
      <title>ADC Channels in LPC54608J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Channels-in-LPC54608J512BD208/m-p/890161#M35687</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;1)&amp;nbsp; I want to use all 12 ADC channels of&amp;nbsp;LPC54608J512BD208 but&amp;nbsp;PIO0_10/ADC0_0,PIO0_11/ADC0_1 and&amp;nbsp;PIO0_12/ADC0_2 are shared with SWD interface pins SWO, SWCLK and SWDIO respectively.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;From datasheet i could see JTAG interface as well in this device. Can i use JTAG debug interface to debug this device as jtag pins&amp;nbsp;are not multiplexed with any of the ADC lines.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) I have OM13092(Revision D) development board for evaluation of LPC54608 microcontroller. Can i test the above point on this development board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jeremyzhou"&gt;jeremyzhou&lt;/A&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/soledad"&gt;soledad&lt;/A&gt;&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ErichS"&gt;ErichS&lt;/A&gt;‌&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 05:14:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Channels-in-LPC54608J512BD208/m-p/890161#M35687</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-05-13T05:14:45Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Channels in LPC54608J512BD208</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Channels-in-LPC54608J512BD208/m-p/890162#M35688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prasanna,&lt;/P&gt;&lt;P&gt;Regarding your question, as far as I know the LPC546xx only supports SWD mode for downloading/debugging code, the JTAG port is ONLY used for JTAG&amp;nbsp; boundary scan function, in other words, you can not use JTAG port to download code and debugging.&lt;/P&gt;&lt;P&gt;I have seen that the SWD signals are multiplexed with ADC0 pins for LPC546xx, I think you can use a jumper to solve the issue, in development stage, you can connect the SWD pins to a connector, while you can use a jumper to connect the SWD pins to ADC analog source. After development phase, you can close the jump, in this way, the SWD pins are ADC pins.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 07:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Channels-in-LPC54608J512BD208/m-p/890162#M35688</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-05-13T07:08:05Z</dc:date>
    </item>
  </channel>
</rss>