<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Initial pull-up state on LPC804</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Initial-pull-up-state-on-LPC804/m-p/888779#M35612</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC804 datasheet (rev. 1.4, page 12) lists PIO0_10 and PIO0_11 as having&amp;nbsp;a passive reset state whereas the remaining GPIO pins have the internal pull-ups enabled by default. The reference manual (UM11065, rev 1.3, page 103-104) lists the reset states of PIO0_10/PIO0_11&amp;nbsp;as also having the pull-&amp;nbsp;ups enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Measuring the pin immediately after the ROM start-up sequence or inspecting the IOCON configuration appears to confirm that the latter behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which document is correct? Are any GPIO I/O pins with a high-Z reset state available on the LPC804M101JHI33E?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 21 Jan 2019 17:00:26 GMT</pubDate>
    <dc:creator>xarowubas</dc:creator>
    <dc:date>2019-01-21T17:00:26Z</dc:date>
    <item>
      <title>Initial pull-up state on LPC804</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Initial-pull-up-state-on-LPC804/m-p/888779#M35612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC804 datasheet (rev. 1.4, page 12) lists PIO0_10 and PIO0_11 as having&amp;nbsp;a passive reset state whereas the remaining GPIO pins have the internal pull-ups enabled by default. The reference manual (UM11065, rev 1.3, page 103-104) lists the reset states of PIO0_10/PIO0_11&amp;nbsp;as also having the pull-&amp;nbsp;ups enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Measuring the pin immediately after the ROM start-up sequence or inspecting the IOCON configuration appears to confirm that the latter behavior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which document is correct? Are any GPIO I/O pins with a high-Z reset state available on the LPC804M101JHI33E?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 17:00:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Initial-pull-up-state-on-LPC804/m-p/888779#M35612</guid>
      <dc:creator>xarowubas</dc:creator>
      <dc:date>2019-01-21T17:00:26Z</dc:date>
    </item>
    <item>
      <title>Re: Initial pull-up state on LPC804</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Initial-pull-up-state-on-LPC804/m-p/888780#M35613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xaro,&lt;/P&gt;&lt;P&gt;This problem was reported and confirmed as a document defect by R&amp;amp;D.&lt;/P&gt;&lt;P&gt;The Datasheet information is typo.&amp;nbsp; Those two GPIO pin are all input / pull-up in reset status.&lt;/P&gt;&lt;P&gt;Our document team will fix it in next release.&lt;/P&gt;&lt;P&gt;Thanks for bringing the problem to our attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 10:17:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Initial-pull-up-state-on-LPC804/m-p/888780#M35613</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-01-24T10:17:49Z</dc:date>
    </item>
  </channel>
</rss>