<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC Sequencing in LPC546xx in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885548#M35501</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I need calrity on the feature that provides interrupt after completion of the sampling of all the cahnnels in the sequence.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;The manual provides details about only single select and burst mode which are not applicable to my application. I want to know the feature that provides this sampling of all channels on 1 trigger and gives an interrupt after completion of sequence.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Apr 2019 08:30:27 GMT</pubDate>
    <dc:creator>prasannanaik</dc:creator>
    <dc:date>2019-04-08T08:30:27Z</dc:date>
    <item>
      <title>ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885544#M35497</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I want to use LPC54605J256BD100 microcontroller in an applicaion where a pulseon an external pin will trigger an ADC and ADC should sample 12 channels on that single pulse input and give output at the end of the sampling of all the 12 channels.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I was going through the user manual of LPC546xx but couldn't find appropriate description for the required functionality. I have follwoing queries regarding Sequencing feature of ADC in LPC546xx:&lt;/P&gt;&lt;P&gt;1) In busrt mode,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;a) Conversion will start after trigger only right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;b) After one sequence(i.e 12 channels sampled), does it stop sampling or initiates a new conversion sequence without any trigger?&lt;/P&gt;&lt;P&gt;&amp;nbsp;2) What is the use of start bit in SEQA_CTRL register?&lt;/P&gt;&lt;P&gt;&amp;nbsp;3) How to acheive the required functionality for my application?&lt;/P&gt;&lt;P&gt;&amp;nbsp;4) Any example code would be helpful&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 05:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885544#M35497</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-04-08T05:00:53Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885545#M35498</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp; Prasanna,&lt;/P&gt;&lt;P&gt;Regarding your question, pls refer to the following:&lt;/P&gt;&lt;P&gt;Q1) In busrt mode,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;a) Conversion will start after trigger only right?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;b) After one sequence(i.e 12 channels sampled), does it stop sampling or initiates a new conversion sequence&lt;/P&gt;&lt;P&gt;without any trigger?&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Burst mode means that the ADC will convert continuously once the ADC is triggered, it do not stop sampling when all 12 channels are sampled. For your application, DO NOT use burst mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q 2) What is the use of start bit in SEQA_CTRL register?&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;The Start bit in SEQA_CTRL register is just used in Software Trigger mode, whne the bit is set by software, ADC convert will be triggered once.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Q3) How to acheive the required functionality for my application?&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Your application requires that the ADC converter is triggered by external signal from GPIO pins, once ADC is triggered, the ADC will sample all 12 channels, then stop sampling, wait for next external trigger signal. I suggest you use the example code in the LPC SDK package:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the case, I think you can modify the void ADC_Configuration(void), change it from software triggering mode to pin hardware triggering mode.&lt;/P&gt;&lt;P&gt;void ADC_Configuration(void)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adc_config_t adcConfigStruct;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adc_conv_seq_config_t adcConvSeqConfigStruct;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Configure the converter. */&lt;BR /&gt;#if defined(FSL_FEATURE_ADC_HAS_CTRL_ASYNMODE) &amp;amp; FSL_FEATURE_ADC_HAS_CTRL_ASYNMODE&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.clockMode = kADC_ClockSynchronousMode; /* Using sync clock source. */&lt;BR /&gt;#endif&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* FSL_FEATURE_ADC_HAS_CTRL_ASYNMODE */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.clockDividerNumber = DEMO_ADC_CLOCK_DIVIDER;&lt;BR /&gt;#if defined(FSL_FEATURE_ADC_HAS_CTRL_RESOL) &amp;amp; FSL_FEATURE_ADC_HAS_CTRL_RESOL&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.resolution = kADC_Resolution12bit;&lt;BR /&gt;#endif /* FSL_FEATURE_ADC_HAS_CTRL_RESOL */&lt;BR /&gt;#if defined(FSL_FEATURE_ADC_HAS_CTRL_BYPASSCAL) &amp;amp; FSL_FEATURE_ADC_HAS_CTRL_BYPASSCAL&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.enableBypassCalibration = false;&lt;BR /&gt;#endif /* FSL_FEATURE_ADC_HAS_CTRL_BYPASSCAL */&lt;BR /&gt;#if defined(FSL_FEATURE_ADC_HAS_CTRL_TSAMP) &amp;amp; FSL_FEATURE_ADC_HAS_CTRL_TSAMP&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.sampleTimeNumber = 0U;&lt;BR /&gt;#endif /* FSL_FEATURE_ADC_HAS_CTRL_TSAMP */&lt;BR /&gt;#if defined(FSL_FEATURE_ADC_HAS_CTRL_LPWRMODE) &amp;amp; FSL_FEATURE_ADC_HAS_CTRL_LPWRMODE&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.enableLowPowerMode = false;&lt;BR /&gt;#endif /* FSL_FEATURE_ADC_HAS_CTRL_LPWRMODE */&lt;BR /&gt;#if defined(FSL_FEATURE_ADC_HAS_TRIM_REG) &amp;amp; FSL_FEATURE_ADC_HAS_TRIM_REG&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConfigStruct.voltageRange = kADC_HighVoltageRange;&lt;BR /&gt;#endif /* FSL_FEATURE_ADC_HAS_TRIM_REG */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_Init(DEMO_ADC_BASE, &amp;amp;adcConfigStruct);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if !(defined(FSL_FEATURE_ADC_HAS_NO_INSEL) &amp;amp;&amp;amp; FSL_FEATURE_ADC_HAS_NO_INSEL)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Use the temperature sensor input to channel 0. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_EnableTemperatureSensor(DEMO_ADC_BASE, true);&lt;BR /&gt;#endif /* FSL_FEATURE_ADC_HAS_NO_INSEL. */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable channel DEMO_ADC_SAMPLE_CHANNEL_NUMBER's conversion in Sequence A. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConvSeqConfigStruct.channelMask =&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (0xFFFU &amp;lt;&amp;lt; DEMO_ADC_SAMPLE_CHANNEL_NUMBER); /* Includes channel DEMO_ADC_SAMPLE_CHANNEL_NUMBER. Rong modified*/&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConvSeqConfigStruct.triggerMask = 1U; //select PIN INT0 as trigger source Rong Wrote&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConvSeqConfigStruct.triggerPolarity = kADC_TriggerPolarityPositiveEdge;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConvSeqConfigStruct.enableSingleStep = false;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConvSeqConfigStruct.enableSyncBypass = false;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; adcConvSeqConfigStruct.interruptMode = kADC_InterruptForEachSequence;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_SetConvSeqAConfig(DEMO_ADC_BASE, &amp;amp;adcConvSeqConfigStruct);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_EnableConvSeqA(DEMO_ADC_BASE, true); /* Enable the conversion sequence A. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Clear the result register. */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_DoSoftwareTriggerConvSeqA(DEMO_ADC_BASE);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while (!ADC_GetChannelConversionResult(DEMO_ADC_BASE, DEMO_ADC_SAMPLE_CHANNEL_NUMBER, &amp;amp;gAdcResultInfoStruct))&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ADC_GetConvSeqAGlobalConversionResult(DEMO_ADC_BASE, &amp;amp;gAdcResultInfoStruct);&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You also need to write the PINTSEL[0] regisyter to select the GPIO pin which can trigger ADC, even you have to configure the pin feature in the IOCON module for the pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Q4) Any example code would be helpful&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;Pls use the ADC example in the SDK package.&lt;/P&gt;&lt;P&gt;You can download SDK package from the link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/welcome" title="https://mcuxpresso.nxp.com/en/welcome"&gt;Welcome | MCUXpresso SDK Builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79779iC09F9FB88C9838F0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 06:41:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885545#M35498</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-04-08T06:41:56Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885546#M35499</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for your valuable input!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;Can you please elaborate your answer for question no. 3. I am not able to find that feature in user manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and best regards,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 06:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885546#M35499</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-04-08T06:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885547#M35500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prasanna,&lt;/P&gt;&lt;P&gt;The ADC supports external pin trigger, pls refer to the following section. For the GINT0/1 module, pls refer to the section:&lt;/P&gt;&lt;P&gt;Chapter 14: LPC546xx Group GPIO input interrupt (GINT0/1)&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/69580iEC5F6DE1411D0B21/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 08:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885547#M35500</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-04-08T08:23:23Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885548#M35501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I need calrity on the feature that provides interrupt after completion of the sampling of all the cahnnels in the sequence.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;The manual provides details about only single select and burst mode which are not applicable to my application. I want to know the feature that provides this sampling of all channels on 1 trigger and gives an interrupt after completion of sequence.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 08:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885548#M35501</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-04-08T08:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885549#M35502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prasanna,&lt;/P&gt;&lt;P&gt;You require&amp;nbsp; the feature that provides interrupt after completion of the sampling of all the cahnnels in the sequence with ONE trigger, okay, this is the bit configuration in SEQA_CTRL/SEQB_CTRL&lt;/P&gt;&lt;P&gt;BURST bit: 0&lt;/P&gt;&lt;P&gt;SINGLESTEP bit: 0&lt;/P&gt;&lt;P&gt;MODE bit: 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 05:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885549#M35502</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-04-09T05:30:12Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885550#M35503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thanks for your guidance. In short SINGLESTEP bit controls the sequencing option. If&amp;nbsp;&lt;SPAN&gt;SINGLESTEP = 1, only one channel will be sampled on trigger and if&amp;nbsp;SINGLESTEP = 0, all channels will be sampled on trigger right?.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Prasanna&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 06:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885550#M35503</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-04-09T06:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885551#M35504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prasanne,&lt;/P&gt;&lt;P&gt;Yes, you are right, &lt;SPAN&gt;if&amp;nbsp;SINGLESTEP = 0, all channels will be sampled on trigger.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Xiangjun Rong&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 07:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885551#M35504</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-04-09T07:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885552#M35505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi XiangJun,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Thank you for solving this query. I have one more query regarding ADC. I couldn't find the effective number of bits in the user manual and data sheet. Could you please help me find it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasanna&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 08:30:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885552#M35505</guid>
      <dc:creator>prasannanaik</dc:creator>
      <dc:date>2019-04-09T08:30:33Z</dc:date>
    </item>
    <item>
      <title>Re: ADC Sequencing in LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885553#M35506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Prasanna,&lt;/P&gt;&lt;P&gt;We have not tested the ENOB(Effective Number of Bits) spec for the ADC of LPC546xx, I am sorry.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Apr 2019 05:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-Sequencing-in-LPC546xx/m-p/885553#M35506</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-04-12T05:06:50Z</dc:date>
    </item>
  </channel>
</rss>