<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No interrupt running Flexcomm in USART-mode with FIFO in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885169#M35463</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem finding information how to receive interrupt when the RX-FIFO in the Flexcomm module is partly filled. When the configured limit in the FIFO is reached, fine, but what if it is not reached. We have experience form the LPC24xx and LPC40xx peripherals where an interrupt is triggered as soon as the flow stopps and the remaining bytes in RX-FIFO can be read out. I have seen solutions with a separate timer but is this the only solution, really? I hope we miss something important!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jan 2019 09:55:40 GMT</pubDate>
    <dc:creator>niklas_swartz</dc:creator>
    <dc:date>2019-01-18T09:55:40Z</dc:date>
    <item>
      <title>No interrupt running Flexcomm in USART-mode with FIFO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885169#M35463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem finding information how to receive interrupt when the RX-FIFO in the Flexcomm module is partly filled. When the configured limit in the FIFO is reached, fine, but what if it is not reached. We have experience form the LPC24xx and LPC40xx peripherals where an interrupt is triggered as soon as the flow stopps and the remaining bytes in RX-FIFO can be read out. I have seen solutions with a separate timer but is this the only solution, really? I hope we miss something important!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 09:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885169#M35463</guid>
      <dc:creator>niklas_swartz</dc:creator>
      <dc:date>2019-01-18T09:55:40Z</dc:date>
    </item>
    <item>
      <title>Re: No interrupt running Flexcomm in USART-mode with FIFO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885170#M35464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="334266" data-username="niklas.swartz@licera.com" href="https://community.nxp.com/people/niklas.swartz@licera.com"&gt;Niklas Swartz&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Actually, I was a bit confused with your question, I'll appreciate a lot if you can tell me which chip you use now.&lt;BR /&gt;Whether you want to implement the same application which is achieved in LPC24xx and LPC40xx in the chip.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 02:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885170#M35464</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-21T02:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: No interrupt running Flexcomm in USART-mode with FIFO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885171#M35465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, OK, sorry for being so unclear.&lt;/P&gt;&lt;P&gt;We have been using the LPC2468/LPC4078 for about 10 years (or more) and using&amp;nbsp;a lot of&amp;nbsp;UART peripherals in our application. We are looking at the LPC540xx or&amp;nbsp; &lt;SPAN&gt;LPC546xx&amp;nbsp;&lt;/SPAN&gt;family that has the Flexcomm design for UART's. We are using FIFO to minimize number of interrupts. In the LPC24xx/LPC40xx uart peripheral there is a CTI (Character Time-out Indicator) that triggers an interrupt if no Rx activity has occurred in 3.5 to 4.5 character time so the fifo can be flushed to application level. So, for example, if the FIFO is configured to trigger an interrupt after 14 received characters and we only received 10 and no more (for a while), the CTI feature will handle this use-case.&lt;BR /&gt;How is this use-case handled in the Flexcomm peripheral design?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 07:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885171#M35465</guid>
      <dc:creator>niklas_swartz</dc:creator>
      <dc:date>2019-01-21T07:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: No interrupt running Flexcomm in USART-mode with FIFO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885172#M35466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="334266" data-username="niklas.swartz@licera.com" href="https://community.nxp.com/people/niklas.swartz@licera.com"&gt;Niklas Swartz&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;Thank you for clarification.&lt;BR /&gt;The CTI feature can provide a 'kind reminder' to read the remaining data in the receive FIFO, what a pity, the LPC54608 doesn't support this feature.&lt;BR /&gt;So I'd like to share a method to achieve the same function.&lt;BR /&gt;The LPC54608 can trigger an interrupt on FIFO receive level reached and the receive level is customized, it's available to receive all the in-coming data stream in the interrupt handler when setting an appropriate receive level.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64206iDDA32479B2BEBC90/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 06:20:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/No-interrupt-running-Flexcomm-in-USART-mode-with-FIFO/m-p/885172#M35466</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-22T06:20:28Z</dc:date>
    </item>
  </channel>
</rss>