<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックWhat's the difference between SIENF and IENF</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-SIENF-and-IENF/m-p/884983#M35450</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a GPIO interrupt working on an LCP11Uxx. There are two registers SIENF and IENF that seem to do the same thing. They both set a bit in IENF. The datasheet says writing to IENF sets an interrupt, and writing to SIENF just writes to IENF. I tested it in the debugger, and it's true.&lt;BR /&gt;&lt;BR /&gt;If I can write directly to IENF, what is the purpose of SIENF?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Feb 2019 19:58:44 GMT</pubDate>
    <dc:creator>lydiaj5000</dc:creator>
    <dc:date>2019-02-22T19:58:44Z</dc:date>
    <item>
      <title>What's the difference between SIENF and IENF</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-SIENF-and-IENF/m-p/884983#M35450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a GPIO interrupt working on an LCP11Uxx. There are two registers SIENF and IENF that seem to do the same thing. They both set a bit in IENF. The datasheet says writing to IENF sets an interrupt, and writing to SIENF just writes to IENF. I tested it in the debugger, and it's true.&lt;BR /&gt;&lt;BR /&gt;If I can write directly to IENF, what is the purpose of SIENF?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Feb 2019 19:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-SIENF-and-IENF/m-p/884983#M35450</guid>
      <dc:creator>lydiaj5000</dc:creator>
      <dc:date>2019-02-22T19:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: What's the difference between SIENF and IENF</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-SIENF-and-IENF/m-p/884984#M35451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a look in the Users Manual:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78368iBEB8B90931E1987F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using IENF you can both set and reset the enable interrupt (writing 0 or 1) in the SIENF you can only enable the interrupt (writing 1), writing a 0 to one of the bits in SIENF has no effect (so you can't&amp;nbsp;by mistake, disable any interrupts that are enabled somewhere else, by setting its bit to 0 in SIENF)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Feb 2019 10:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/What-s-the-difference-between-SIENF-and-IENF/m-p/884984#M35451</guid>
      <dc:creator>carstengroen</dc:creator>
      <dc:date>2019-02-23T10:10:22Z</dc:date>
    </item>
  </channel>
</rss>