<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Flashing to lpc2378 using flashmagic</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-to-lpc2378-using-flashmagic/m-p/881321#M35255</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chandrika,&lt;/P&gt;&lt;P&gt;It seems that you need to force entering into bootloader mode before running your application (that uses the same UART). Please refer to the following links for additional details and troubleshooting:&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.flashmagictool.com/index.php?topic=3424.0"&gt;http://forum.flashmagictool.com/index.php?topic=3424.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.flashmagictool.com/index.php?topic=3628.0"&gt;http://forum.flashmagictool.com/index.php?topic=3628.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Feb 2019 18:46:25 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2019-02-06T18:46:25Z</dc:date>
    <item>
      <title>Flashing to lpc2378 using flashmagic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-to-lpc2378-using-flashmagic/m-p/881320#M35254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My project need to transmit a string using uart and also to receive data. I had flashed my program( i have used interrupts) to board and it continously prints 'p'. Now i am not able to flash corrected program to board.i am using com port 0 to flash and the same port to transmit and receive data. Manual reset on board is also giving no any impact. Please help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Feb 2019 10:48:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-to-lpc2378-using-flashmagic/m-p/881320#M35254</guid>
      <dc:creator>chandrika1643</dc:creator>
      <dc:date>2019-02-02T10:48:41Z</dc:date>
    </item>
    <item>
      <title>Re: Flashing to lpc2378 using flashmagic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-to-lpc2378-using-flashmagic/m-p/881321#M35255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chandrika,&lt;/P&gt;&lt;P&gt;It seems that you need to force entering into bootloader mode before running your application (that uses the same UART). Please refer to the following links for additional details and troubleshooting:&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.flashmagictool.com/index.php?topic=3424.0"&gt;http://forum.flashmagictool.com/index.php?topic=3424.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://forum.flashmagictool.com/index.php?topic=3628.0"&gt;http://forum.flashmagictool.com/index.php?topic=3628.0&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Feb 2019 18:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Flashing-to-lpc2378-using-flashmagic/m-p/881321#M35255</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-02-06T18:46:25Z</dc:date>
    </item>
  </channel>
</rss>