<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC51U68 min USB VDD 3V</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879256#M35143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Section 13.6 fig 33 VBUS(1) is combination that I want. Question is if in case of VDD=1.8V USB (CDC device) can work or not? Because in table 12 (10.1 General operating conditions) there is min 3.0V VDD specified for USB operation only!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Feb 2019 10:21:52 GMT</pubDate>
    <dc:creator>jh0</dc:creator>
    <dc:date>2019-02-07T10:21:52Z</dc:date>
    <item>
      <title>LPC51U68 min USB VDD 3V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879254#M35141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any way to use LPC51U68 USB with 1.8V VDD. If not, is there any similar device (M0+ 100MHz) with this possibility.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Feb 2019 11:46:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879254#M35141</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2019-02-02T11:46:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 min USB VDD 3V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879255#M35142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the LPC51U68 it is one self-power supply, as you can review in the datasheet of the device Section 13.6 Suggested USB Interface Solutions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;TIC Support Team&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Feb 2019 21:09:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879255#M35142</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-02-06T21:09:50Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 min USB VDD 3V</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879256#M35143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In Section 13.6 fig 33 VBUS(1) is combination that I want. Question is if in case of VDD=1.8V USB (CDC device) can work or not? Because in table 12 (10.1 General operating conditions) there is min 3.0V VDD specified for USB operation only!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2019 10:21:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-min-USB-VDD-3V/m-p/879256#M35143</guid>
      <dc:creator>jh0</dc:creator>
      <dc:date>2019-02-07T10:21:52Z</dc:date>
    </item>
  </channel>
</rss>