<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The code in M0 core is running from SRAM or FLASH? (LPC54114) in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-code-in-M0-core-is-running-from-SRAM-or-FLASH-LPC54114/m-p/878322#M35129</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm now running a dual-core project in LPC54114. Every thing works fine. But it came to me that from where the M0 core fetched its code? SRAM or FLASH? What about M4?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 10:10:31 GMT</pubDate>
    <dc:creator>da_chen</dc:creator>
    <dc:date>2019-03-21T10:10:31Z</dc:date>
    <item>
      <title>The code in M0 core is running from SRAM or FLASH? (LPC54114)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-code-in-M0-core-is-running-from-SRAM-or-FLASH-LPC54114/m-p/878322#M35129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm now running a dual-core project in LPC54114. Every thing works fine. But it came to me that from where the M0 core fetched its code? SRAM or FLASH? What about M4?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 10:10:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-code-in-M0-core-is-running-from-SRAM-or-FLASH-LPC54114/m-p/878322#M35129</guid>
      <dc:creator>da_chen</dc:creator>
      <dc:date>2019-03-21T10:10:31Z</dc:date>
    </item>
    <item>
      <title>Re: The code in M0 core is running from SRAM or FLASH? (LPC54114)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/The-code-in-M0-core-is-running-from-SRAM-or-FLASH-LPC54114/m-p/878323#M35130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The M0+ core slave project is distributed in RAM. The slave project is associated with the master project. So, it will be compiled first and then the image data will be linked into the master image file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So after power on, the slave fetch code from flash to RAM then run code from RAM.&lt;/P&gt;&lt;P&gt;The M4 core run project from Flash.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Mar 2019 07:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/The-code-in-M0-core-is-running-from-SRAM-or-FLASH-LPC54114/m-p/878323#M35130</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-03-22T07:34:23Z</dc:date>
    </item>
  </channel>
</rss>