<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC54608 and Flash Magic in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-and-Flash-Magic/m-p/876313#M35041</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I could program LPC54608&amp;nbsp;by Flash Magic(USART mode).&lt;/P&gt;&lt;P&gt;But it is free software.&lt;/P&gt;&lt;P&gt;Can I use flash magic for a programming of a product?&lt;/P&gt;&lt;P&gt;okuyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Apr 2019 07:39:27 GMT</pubDate>
    <dc:creator>実奥山</dc:creator>
    <dc:date>2019-04-03T07:39:27Z</dc:date>
    <item>
      <title>LPC54608 and Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-and-Flash-Magic/m-p/876313#M35041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I could program LPC54608&amp;nbsp;by Flash Magic(USART mode).&lt;/P&gt;&lt;P&gt;But it is free software.&lt;/P&gt;&lt;P&gt;Can I use flash magic for a programming of a product?&lt;/P&gt;&lt;P&gt;okuyama&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2019 07:39:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-and-Flash-Magic/m-p/876313#M35041</guid>
      <dc:creator>実奥山</dc:creator>
      <dc:date>2019-04-03T07:39:27Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54608 and Flash Magic</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-and-Flash-Magic/m-p/876314#M35042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="309825" data-username="実奥山" href="https://community.nxp.com/people/実奥山"&gt;実 奥山&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Do you mean you want to program your product (based on LPC54608) ?&lt;/P&gt;&lt;P&gt;If yes, sure, you can .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 09:52:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54608-and-Flash-Magic/m-p/876314#M35042</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-04-04T09:52:31Z</dc:date>
    </item>
  </channel>
</rss>