<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: how to create a .nnc.bin file ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875774#M35017</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I make a test firmware, and create a .bin file, and I'd like to make use of the CLRC663 Evaluation board's "Secondary Firmware options" feature, and load my test firmware into the on-board LPC1769 MCU's secondary firmware. &lt;BR /&gt;I suppose it will not erase the LPC1769 MCU's existing firmware, which works with NFC Cockpit PC program.&lt;BR /&gt;However, when I try to "Load Secondary Firmware", the Cockpit's user interface shows that it is looking for the firmware file end with .nnc.bin.&lt;BR /&gt;So, what can I do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jan 2019 01:52:33 GMT</pubDate>
    <dc:creator>yyluk</dc:creator>
    <dc:date>2019-01-18T01:52:33Z</dc:date>
    <item>
      <title>how to create a .nnc.bin file ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875772#M35015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;how to create a .nnc.bin file ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 08:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875772#M35015</guid>
      <dc:creator>yyluk</dc:creator>
      <dc:date>2019-01-15T08:38:58Z</dc:date>
    </item>
    <item>
      <title>Re: how to create a .nnc.bin file ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875773#M35016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;When building a project, the MCUXpresso IDE tools create an ARM executable format (AXF) file – which is actually standard ELF/DWARF file. This file can be programmed directly down to your target using the MCUXpresso IDE debug functionality, but it may also be converted into a variety of formats suitable for use in other external tools.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information about&amp;nbsp;Creating bin, hex or S-Record files or conversions within the IDE, please check chapter 19.10 of the&amp;nbsp;MCUXpresso IDE User Guide.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf" title="https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf"&gt;https://www.nxp.com/docs/en/user-guide/MCUXpresso_IDE_User_Guide.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 15:34:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875773#M35016</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-01-16T15:34:25Z</dc:date>
    </item>
    <item>
      <title>Re: how to create a .nnc.bin file ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875774#M35017</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I make a test firmware, and create a .bin file, and I'd like to make use of the CLRC663 Evaluation board's "Secondary Firmware options" feature, and load my test firmware into the on-board LPC1769 MCU's secondary firmware. &lt;BR /&gt;I suppose it will not erase the LPC1769 MCU's existing firmware, which works with NFC Cockpit PC program.&lt;BR /&gt;However, when I try to "Load Secondary Firmware", the Cockpit's user interface shows that it is looking for the firmware file end with .nnc.bin.&lt;BR /&gt;So, what can I do ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 01:52:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/how-to-create-a-nnc-bin-file/m-p/875774#M35017</guid>
      <dc:creator>yyluk</dc:creator>
      <dc:date>2019-01-18T01:52:33Z</dc:date>
    </item>
  </channel>
</rss>