<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSuggest to add reading function for ISER on LPCOpen</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Suggest-to-add-reading-function-for-ISER-on-LPCOpen/m-p/875439#M34998</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to user manual of LPC11U6X and this post&amp;nbsp;&lt;A href="https://community.nxp.com/thread/421105"&gt;LPC11 - interrupts during IAP&lt;/A&gt;&amp;nbsp;, SW needs to temporarily disable interrupt before using IAP calls. My idea is to&amp;nbsp;(1) backup ISER0 (2) write all-one to ICER0 (3) IAP-call (4) Write backup-value back to&amp;nbsp;&lt;SPAN&gt;ISER0. However, without relevant function SW can only read it from register directly.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it possible to add API to read ISER so that SW can read it without direct-accessing register?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jeremy&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Jan 2019 04:00:38 GMT</pubDate>
    <dc:creator>jeremyhsiao</dc:creator>
    <dc:date>2019-01-15T04:00:38Z</dc:date>
    <item>
      <title>Suggest to add reading function for ISER on LPCOpen</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Suggest-to-add-reading-function-for-ISER-on-LPCOpen/m-p/875439#M34998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to user manual of LPC11U6X and this post&amp;nbsp;&lt;A href="https://community.nxp.com/thread/421105"&gt;LPC11 - interrupts during IAP&lt;/A&gt;&amp;nbsp;, SW needs to temporarily disable interrupt before using IAP calls. My idea is to&amp;nbsp;(1) backup ISER0 (2) write all-one to ICER0 (3) IAP-call (4) Write backup-value back to&amp;nbsp;&lt;SPAN&gt;ISER0. However, without relevant function SW can only read it from register directly.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is it possible to add API to read ISER so that SW can read it without direct-accessing register?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;BR&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Jeremy&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Jan 2019 04:00:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Suggest-to-add-reading-function-for-ISER-on-LPCOpen/m-p/875439#M34998</guid>
      <dc:creator>jeremyhsiao</dc:creator>
      <dc:date>2019-01-15T04:00:38Z</dc:date>
    </item>
    <item>
      <title>Re: Suggest to add reading function for ISER on LPCOpen</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Suggest-to-add-reading-function-for-ISER-on-LPCOpen/m-p/875440#M34999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy Hsiao,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, you don't need to read out the ISER and clear ICER, you can just do it like the lpcopen periph_flashiap project.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Before you do the IAP call, you disable the interrupt with this code:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __disable_irq();&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; After you finish the IAP function, you can enable the interrupt with this code:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; __enable_irq();&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63594i39E904A5A24571F2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question about it, please kindly let me know.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 03:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Suggest-to-add-reading-function-for-ISER-on-LPCOpen/m-p/875440#M34999</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2019-01-17T03:25:11Z</dc:date>
    </item>
  </channel>
</rss>