<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCan USB be connected when LPC54114 is in deep-sleep mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB-be-connected-when-LPC54114-is-in-deep-sleep-mode/m-p/874828#M34896</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found that USB can be set to wake up the MCU when in deep-sleep mode. But what if I disable the wake up interruption from USB. Do I need to reconnect with other devices? Or if I don't shutdown the USB connection, but block the interruption, will the MCU still be waked up by USB in deep-sleep mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Mar 2019 05:37:52 GMT</pubDate>
    <dc:creator>da_chen</dc:creator>
    <dc:date>2019-03-07T05:37:52Z</dc:date>
    <item>
      <title>Can USB be connected when LPC54114 is in deep-sleep mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB-be-connected-when-LPC54114-is-in-deep-sleep-mode/m-p/874828#M34896</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found that USB can be set to wake up the MCU when in deep-sleep mode. But what if I disable the wake up interruption from USB. Do I need to reconnect with other devices? Or if I don't shutdown the USB connection, but block the interruption, will the MCU still be waked up by USB in deep-sleep mode?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Mar 2019 05:37:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB-be-connected-when-LPC54114-is-in-deep-sleep-mode/m-p/874828#M34896</guid>
      <dc:creator>da_chen</dc:creator>
      <dc:date>2019-03-07T05:37:52Z</dc:date>
    </item>
    <item>
      <title>Re: Can USB be connected when LPC54114 is in deep-sleep mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB-be-connected-when-LPC54114-is-in-deep-sleep-mode/m-p/874829#M34897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Da Chen,&lt;/P&gt;&lt;P&gt;USB interrupt can wake up MCU from deep sleep mode. In order to utilize it, you need enable USB NEEDCLK interrupt.&lt;/P&gt;&lt;P&gt;Besides, you need also enable the USB activity wake-up interrupt in the NVIC.&lt;/P&gt;&lt;P&gt;For more information, see UM10914 LPC5411X user manual, 22.7.6 USB wake-up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 06:53:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-USB-be-connected-when-LPC54114-is-in-deep-sleep-mode/m-p/874829#M34897</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-03-11T06:53:09Z</dc:date>
    </item>
  </channel>
</rss>