<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックSSP Demo Example is failing at buffer verify for LPC 1837</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-Demo-Example-is-failing-at-buffer-verify-for-LPC-1837/m-p/869957#M34690</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am using LPC 1837 controller and using Expresso IDE.I am trying to run the SSP demo example for SPI on two LPC boards.Following are my connections for that&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Board 1:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt;Configured as Master.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.5 as SSEL&amp;nbsp;&lt;SPAN&gt;which is connected to&amp;nbsp;SSEL on other LPC 1837 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; PF.4 as SCK1&amp;nbsp;&lt;SPAN&gt;which is connected to&amp;nbsp;SCLK on other LPC 1837 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.4 as MOSI which is connected to MISO on other LPC 1837 board.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.3 as MISO&amp;nbsp;&lt;SPAN&gt;which is connected to MOSI on other LPC 1837 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Board 2:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;=&amp;gt;Configured as Slave.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.5 as SSEL&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; PF.4 as SCK1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.4 as MOSI&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.3 as MISO&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;When I am running the demo application on both the boards and I am getting always &lt;STRONG&gt;buffer_verify()&lt;/STRONG&gt; failure.Do I need to do anything beyond these connections or anything to be added in the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;srikanth.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 05:50:14 GMT</pubDate>
    <dc:creator>srikanthmediset</dc:creator>
    <dc:date>2019-01-11T05:50:14Z</dc:date>
    <item>
      <title>SSP Demo Example is failing at buffer verify for LPC 1837</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-Demo-Example-is-failing-at-buffer-verify-for-LPC-1837/m-p/869957#M34690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am using LPC 1837 controller and using Expresso IDE.I am trying to run the SSP demo example for SPI on two LPC boards.Following are my connections for that&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Board 1:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt;Configured as Master.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.5 as SSEL&amp;nbsp;&lt;SPAN&gt;which is connected to&amp;nbsp;SSEL on other LPC 1837 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; PF.4 as SCK1&amp;nbsp;&lt;SPAN&gt;which is connected to&amp;nbsp;SCLK on other LPC 1837 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.4 as MOSI which is connected to MISO on other LPC 1837 board.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.3 as MISO&amp;nbsp;&lt;SPAN&gt;which is connected to MOSI on other LPC 1837 board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Board 2:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;=&amp;gt;Configured as Slave.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.5 as SSEL&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; PF.4 as SCK1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.4 as MOSI&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; =&amp;gt; P1.3 as MISO&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;When I am running the demo application on both the boards and I am getting always &lt;STRONG&gt;buffer_verify()&lt;/STRONG&gt; failure.Do I need to do anything beyond these connections or anything to be added in the code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;srikanth.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 05:50:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-Demo-Example-is-failing-at-buffer-verify-for-LPC-1837/m-p/869957#M34690</guid>
      <dc:creator>srikanthmediset</dc:creator>
      <dc:date>2019-01-11T05:50:14Z</dc:date>
    </item>
    <item>
      <title>Re: SSP Demo Example is failing at buffer verify for LPC 1837</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-Demo-Example-is-failing-at-buffer-verify-for-LPC-1837/m-p/869958#M34691</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="302217" data-username="srikanthmedisetty" href="https://community.nxp.com/people/srikanthmedisetty"&gt;Srikanth Medisetty&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd highly recommend you to refer the attachment which contains the master_SSP and slave_SSP demo。&lt;BR /&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Jan 2019 02:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SSP-Demo-Example-is-failing-at-buffer-verify-for-LPC-1837/m-p/869958#M34691</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-14T02:52:51Z</dc:date>
    </item>
  </channel>
</rss>