<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB_VBUS and USB1_VBUS in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-VBUS-and-USB1-VBUS/m-p/869520#M34673</link>
    <description>&lt;P&gt;Hi, Maki,&lt;/P&gt;
&lt;P&gt;Q1)When USB1_AVDD3V3, USB1_AVDDTX3V3 and VDD are connected to 3.3V LDO, is USB1_VBUS 5V tolerant?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;yes, the USB1_VBUS is an digital signal input pin for LPC546xx family, the USB1_VBUS 5V tolerant means that the pin can accept both 5V logic and 3.3V logic signal. When USB1_AVDD3V3, USB1_AVDDTX3V3 and VDD are connected to 3.3V LDO,&amp;nbsp; USB1_VBUS is 5V tolerant.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Q2)I have another question about VBUS, If USB1 is only used for host mode, should it be connected to VDD instead of VBUS according to table 5. termination of unused pins?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;If the USB1 is only used for host mode, and the host USB1 connector provide 5V power for the USB device which inserted into the USB1 connector, in the case, I suppose that the VDD power supply(3.3V) is from the 5V power supply via a regulator, the USB1_VBUS signal pin is not used, you can connect to either VDD or GND or float.&lt;/P&gt;
&lt;P&gt;Pls refer to section 13.7 in data sheet.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;
&lt;P&gt;13.7 Suggested USB interface solutions&lt;BR /&gt;The USB device can be connected to the USB as self-powered device (see Figure 48) or&lt;BR /&gt;bus-powered device (see Figure 49).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"&lt;BR /&gt;On the LPC546xx, the USB_VBUS pin is 5 V tolerant only when VDD is applied and at&lt;BR /&gt;operating voltage level. Therefore, if the USB_VBUS function is connected to the USB&lt;BR /&gt;connector and the device is self-powered, the USB_VBUS pin must be protected for&lt;BR /&gt;situations when VDD = 0 V.&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;PLS note above line.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;If VDD is always at operating level while VBUS = 5 V, the USB_VBUS pin can be&lt;BR /&gt;connected directly to the VBUS pin on the USB connector.&lt;BR /&gt;For systems where VDD can be 0 V and VBUS is directly applied to the VBUS pin,&lt;BR /&gt;precautions must be taken to reduce the voltage to below 3.6 V, which is the maximum&lt;BR /&gt;allowable voltage on the USB_VBUS pin in this case.&lt;BR /&gt;One method is to use a voltage divider to connect the USB_VBUS pin to the VBUS on the&lt;BR /&gt;USB connector. The voltage divider ratio should be such that the USB_VBUS pin is&lt;BR /&gt;greater than 0.7 VDD to indicate a logic HIGH while below the 3.6 V allowable maximum&lt;BR /&gt;voltage.&lt;BR /&gt;For the following operating conditions&lt;BR /&gt;VBUSmax = 5.25 V&lt;BR /&gt;VDD = 3.6 V,&lt;BR /&gt;the voltage divider should provide a reduction of 3.6 V/5.25 V or ~0.686 V.&lt;/P&gt;</description>
    <pubDate>Fri, 24 May 2024 06:28:00 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2024-05-24T06:28:00Z</dc:date>
    <item>
      <title>USB_VBUS and USB1_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-VBUS-and-USB1-VBUS/m-p/869519#M34672</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LPC546xx datasheet says as follows.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61866i8C1C885595B50D7E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61916i89EDF3B2E014E898/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When USB1_AVDD3V3, USB1_AVDDTX3V3 and VDD are connected to 3.3V LDO, is USB1_VBUS 5V tolerant?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have another question about VBUS, If USB1 is only used for host mode, should it be connected to VDD instead of VBUS according to table 5. termination of unused pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 12:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-VBUS-and-USB1-VBUS/m-p/869519#M34672</guid>
      <dc:creator>hirai</dc:creator>
      <dc:date>2019-03-19T12:32:59Z</dc:date>
    </item>
    <item>
      <title>Re: USB_VBUS and USB1_VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-VBUS-and-USB1-VBUS/m-p/869520#M34673</link>
      <description>&lt;P&gt;Hi, Maki,&lt;/P&gt;
&lt;P&gt;Q1)When USB1_AVDD3V3, USB1_AVDDTX3V3 and VDD are connected to 3.3V LDO, is USB1_VBUS 5V tolerant?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;yes, the USB1_VBUS is an digital signal input pin for LPC546xx family, the USB1_VBUS 5V tolerant means that the pin can accept both 5V logic and 3.3V logic signal. When USB1_AVDD3V3, USB1_AVDDTX3V3 and VDD are connected to 3.3V LDO,&amp;nbsp; USB1_VBUS is 5V tolerant.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Q2)I have another question about VBUS, If USB1 is only used for host mode, should it be connected to VDD instead of VBUS according to table 5. termination of unused pins?&lt;/P&gt;
&lt;P&gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;&amp;gt;If the USB1 is only used for host mode, and the host USB1 connector provide 5V power for the USB device which inserted into the USB1 connector, in the case, I suppose that the VDD power supply(3.3V) is from the 5V power supply via a regulator, the USB1_VBUS signal pin is not used, you can connect to either VDD or GND or float.&lt;/P&gt;
&lt;P&gt;Pls refer to section 13.7 in data sheet.&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Xiangjun Rong&lt;/P&gt;
&lt;P&gt;13.7 Suggested USB interface solutions&lt;BR /&gt;The USB device can be connected to the USB as self-powered device (see Figure 48) or&lt;BR /&gt;bus-powered device (see Figure 49).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;"&lt;BR /&gt;On the LPC546xx, the USB_VBUS pin is 5 V tolerant only when VDD is applied and at&lt;BR /&gt;operating voltage level. Therefore, if the USB_VBUS function is connected to the USB&lt;BR /&gt;connector and the device is self-powered, the USB_VBUS pin must be protected for&lt;BR /&gt;situations when VDD = 0 V.&lt;/P&gt;
&lt;P&gt;"&lt;/P&gt;
&lt;P&gt;PLS note above line.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;If VDD is always at operating level while VBUS = 5 V, the USB_VBUS pin can be&lt;BR /&gt;connected directly to the VBUS pin on the USB connector.&lt;BR /&gt;For systems where VDD can be 0 V and VBUS is directly applied to the VBUS pin,&lt;BR /&gt;precautions must be taken to reduce the voltage to below 3.6 V, which is the maximum&lt;BR /&gt;allowable voltage on the USB_VBUS pin in this case.&lt;BR /&gt;One method is to use a voltage divider to connect the USB_VBUS pin to the VBUS on the&lt;BR /&gt;USB connector. The voltage divider ratio should be such that the USB_VBUS pin is&lt;BR /&gt;greater than 0.7 VDD to indicate a logic HIGH while below the 3.6 V allowable maximum&lt;BR /&gt;voltage.&lt;BR /&gt;For the following operating conditions&lt;BR /&gt;VBUSmax = 5.25 V&lt;BR /&gt;VDD = 3.6 V,&lt;BR /&gt;the voltage divider should provide a reduction of 3.6 V/5.25 V or ~0.686 V.&lt;/P&gt;</description>
      <pubDate>Fri, 24 May 2024 06:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-VBUS-and-USB1-VBUS/m-p/869520#M34673</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-05-24T06:28:00Z</dc:date>
    </item>
  </channel>
</rss>