<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Internal eeprom code for lpc2134</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869379#M34662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The LPC2134 device doesn’t have internal EEPROM. It has internal Flash with In-Application-Programming (IAP) capabilities, that could be used for storing non-volatile variables.&lt;/P&gt;&lt;P&gt;For additional details regarding this you could refer to application note AN10256 "Using IAP for LPC2000 Arm devices” at the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN10256.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN10256.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Jan 2019 22:42:51 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2019-01-11T22:42:51Z</dc:date>
    <item>
      <title>Internal eeprom code for lpc2134</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869378#M34661</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi i am working on a program where i need to store variables and arrays in internal eeprom so that after reset of MCU i cn access them and again rewrite them&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using lpc2134 controller. need a sample code for storing variable to internal eeprom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 03:38:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869378#M34661</guid>
      <dc:creator>bilal6043</dc:creator>
      <dc:date>2019-01-11T03:38:31Z</dc:date>
    </item>
    <item>
      <title>Re: Internal eeprom code for lpc2134</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869379#M34662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The LPC2134 device doesn’t have internal EEPROM. It has internal Flash with In-Application-Programming (IAP) capabilities, that could be used for storing non-volatile variables.&lt;/P&gt;&lt;P&gt;For additional details regarding this you could refer to application note AN10256 "Using IAP for LPC2000 Arm devices” at the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN10256.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN10256.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 22:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869379#M34662</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-01-11T22:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: Internal eeprom code for lpc2134</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869380#M34663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi carlos.. thanks for the reply.. i use this sample in my application... i need to ask if i reset the micro controller (reset power) variable still stored inside internal flash?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jan 2019 01:44:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869380#M34663</guid>
      <dc:creator>bilal6043</dc:creator>
      <dc:date>2019-01-12T01:44:51Z</dc:date>
    </item>
    <item>
      <title>Re: Internal eeprom code for lpc2134</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869381#M34664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also if you could provide some light on the example code by nxp ... as for me its not stroing any values in flash.. or may i am not getting it right&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Jan 2019 02:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Internal-eeprom-code-for-lpc2134/m-p/869381#M34664</guid>
      <dc:creator>bilal6043</dc:creator>
      <dc:date>2019-01-12T02:18:52Z</dc:date>
    </item>
  </channel>
</rss>