<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC51U68 I2S Spec</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869322#M34641</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ian,&lt;/P&gt;&lt;P&gt;For the LPC51U68 processor, there are two independent instances of an I2S interface:&lt;/P&gt;&lt;P&gt;One instance:&lt;/P&gt;&lt;P&gt;PIO0_5: FC6_RXD_SDA_MOSI_DATA&lt;BR /&gt;PIO0_6: FC6_TXD_SCL_MISO_WS &lt;BR /&gt;PIO0_7: FC6_SCK &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another instance:&lt;/P&gt;&lt;P&gt;PIO1_12: FC7_SCK&lt;BR /&gt;PIO1_13: FC7_RXD_SDA_MOSI_DATA&lt;BR /&gt;PIO1_14: FC7_TXD_SCL_MISO_WS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, one instance can be connected to Codec ADC, another instance can be connected to Codec DAC. You can use I2S mode or TDM modes, for the I2S mode, there are two slots, for the TDM mode, the maximum frame length is 512 bits, in other words, the maximum slots is 512/32=16, so there are 8 channel pairs or 16 slots at most.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Feb 2019 03:17:46 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-02-20T03:17:46Z</dc:date>
    <item>
      <title>LPC51U68 I2S Spec</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869321#M34640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There doesn't even seem to be a section for LPC51 yet, so I put it in here.&lt;/P&gt;&lt;P&gt;If I was to connect the device to a codec with several input and output channels, how many can it support?&lt;BR /&gt;Reading the manual, it seems to have two instances of an I2S interface, but each is capable of being and input OR an output but not both; so I'd need both of them to connect to a codec with both ADCs and DACs. Is that correct?&lt;/P&gt;&lt;P&gt;Most codecs seem to communicate using TDM with one time-slot per input/output. What is the maximum number of timeslots? It seems from the manual it is limited to 512 bits per sample in total, 256 left and 256 right, so 8 channels of 32 bits, perhaps?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Feb 2019 13:39:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869321#M34640</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2019-02-17T13:39:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 I2S Spec</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869322#M34641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Ian,&lt;/P&gt;&lt;P&gt;For the LPC51U68 processor, there are two independent instances of an I2S interface:&lt;/P&gt;&lt;P&gt;One instance:&lt;/P&gt;&lt;P&gt;PIO0_5: FC6_RXD_SDA_MOSI_DATA&lt;BR /&gt;PIO0_6: FC6_TXD_SCL_MISO_WS &lt;BR /&gt;PIO0_7: FC6_SCK &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Another instance:&lt;/P&gt;&lt;P&gt;PIO1_12: FC7_SCK&lt;BR /&gt;PIO1_13: FC7_RXD_SDA_MOSI_DATA&lt;BR /&gt;PIO1_14: FC7_TXD_SCL_MISO_WS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, one instance can be connected to Codec ADC, another instance can be connected to Codec DAC. You can use I2S mode or TDM modes, for the I2S mode, there are two slots, for the TDM mode, the maximum frame length is 512 bits, in other words, the maximum slots is 512/32=16, so there are 8 channel pairs or 16 slots at most.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 03:17:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869322#M34641</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-02-20T03:17:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 I2S Spec</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869323#M34642</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Feb 2019 10:39:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-I2S-Spec/m-p/869323#M34642</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2019-02-20T10:39:30Z</dc:date>
    </item>
  </channel>
</rss>