<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC82X PIO0_4 as output</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869304#M34639</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for sharing.&lt;/P&gt;&lt;P&gt;This has happened to me before, I looked at it for hours and didn't see it.&lt;/P&gt;&lt;P&gt;One thing that helps, when you are sufficiently desperate, is to look at the generated assembly code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Apr 2019 12:21:26 GMT</pubDate>
    <dc:creator>starblue</dc:creator>
    <dc:date>2019-04-01T12:21:26Z</dc:date>
    <item>
      <title>LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869292#M34627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use PIO0_4 as output on a LPC824, but I am missing something. There are no problems with other pins. &lt;/P&gt;&lt;P&gt;There is a statement in the datasheet rev 1.3 on page 10 - note 3 in Table 3, pin description - "The wake-up pin function can be disabled and the pin can be used for other purposes, if the WKT low-power oscillator is enabled for waking up the part from Deep power-down mode."&lt;/P&gt;&lt;P&gt;ADC11 is switched off in PINENABLE&lt;/P&gt;&lt;P&gt;I have tried to put value 2 in DPDCTRL, but that doesn't make any difference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Pin seems to be input with pullup.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 13:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869292#M34627</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2019-03-19T13:46:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869293#M34628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="284524" data-username="kurtmirdell" href="https://community.nxp.com/people/kurtmirdell"&gt;Kurt Mirdell&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;I think you forgot to configure the MODE bits in the PIO0_4 register.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/64289i7A7EA2044955DDE9/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 03:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869293#M34628</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-03-20T03:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869294#M34629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the pin as output. The pin is now input with pull-up as I described in the question. Your suggestion is the default for the pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 22:49:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869294#M34629</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2019-03-26T22:49:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869295#M34630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="284524" data-username="kurtmirdell" href="https://community.nxp.com/people/kurtmirdell"&gt;Kurt Mirdell&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;BR /&gt;Actually, you should configure the MODE bits of PIO_4 to be 0x00 instead of the 0x02.&lt;BR /&gt;Please give a try.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2019 07:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869295#M34630</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-03-27T07:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869296#M34631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tested your suggestion, but it doesn't change anything. PIO0_4 is not working as output regardless of pull-up selections.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to my understanding, you enable the output in the direction registers (DIR/DIRSET/DIRCLR/DIRNOT). The pull-up enabling does not affect output enabling, but it is a little stupid to have pull-ups enabled on an output.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I am looking for is the secret, not so well documented thing that you need to do to use PIO0_4 as an output instead of the WAKEPAD function.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2019 11:48:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869296#M34631</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2019-03-27T11:48:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869297#M34632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="284524" data-username="kurtmirdell" href="https://community.nxp.com/people/kurtmirdell"&gt;Kurt Mirdell&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;BR /&gt;It seems a bit weird.&lt;BR /&gt;I'd like to replicate the phenomenon on my site, so whether you can share a compile-able demo, then I'll run it with the LPCXpresso 804 board for testing.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 08:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869297#M34632</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-03-28T08:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869298#M34633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a fully functional software for a special hardware. I don't think it would be any good if you try that on some other hardware. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My tests has been made both by additions to my software and also by direct manipulating things in my monitoring software where I can access all memory and ports.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to my understanding, you should do the following to set a PIO_4 to output:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bit 24 in PINENABLE0, address 0x4000 C1C0, should be 1 but that is default on reset so it should not be necessary to change.&lt;/P&gt;&lt;P&gt;Enable GPIO clock (bit 6) in SYSAHBCLKCTRL, address 0x4004 8080, also default on reset.&lt;/P&gt;&lt;P&gt;Set port as output by writing a 1 in correct position (0x10 for PIO_4) in GPIO direction port register (DIR0, address 0xA000 2000)&lt;/P&gt;&lt;P&gt;Pin should now be output and should be possible to set to 0/1 by writing 0/0x10 to GPIO port pin register (PIN0, address 0xA000 2100)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have checked actual register contents.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this has something to do with the wake-up pin functionality on this pin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 09:21:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869298#M34633</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2019-03-28T09:21:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869299#M34634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found the problem, bit 24 in PINENABLE was actually 0. Works as it should. However, the wording in the manual about wake-up function made me believe that that was the problem. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 12:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869299#M34634</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2019-03-28T12:04:51Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869300#M34635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In LPC82x ISP uses P0_4 as U0_TXD,&amp;nbsp; have you checked whether that is still the case?&lt;/P&gt;&lt;P&gt;Or more generally, whether some other function is mapped to P0_4 via PINASSIGN?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 12:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869300#M34635</guid>
      <dc:creator>starblue</dc:creator>
      <dc:date>2019-03-28T12:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869301#M34636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="284524" data-username="kurtmirdell" href="https://community.nxp.com/people/kurtmirdell"&gt;Kurt Mirdell&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your reply.&lt;BR /&gt;I've used the lpcxpresso804_led_blinky demo which is from the SDK library as the template, and do a bit modification to make the PIO0_4&amp;nbsp; toggles per 1 second.&lt;BR /&gt;It works well, please check the attachment and give a try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="新建文件1.bmp"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62955i036B3E098A000BBE/image-size/large?v=v2&amp;amp;px=999" role="button" title="新建文件1.bmp" alt="新建文件1.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;Fig 1&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="WeChat Image_20190329150958.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62987iDC0D42B22AF4D8B0/image-size/large?v=v2&amp;amp;px=999" role="button" title="WeChat Image_20190329150958.jpg" alt="WeChat Image_20190329150958.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;Fig 2&lt;/P&gt;&lt;P style="text-align: left;"&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Mar 2019 07:11:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869301#M34636</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-03-29T07:11:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869302#M34637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem was actually a software problem.&lt;/P&gt;&lt;P&gt;I had a statement that was&lt;/P&gt;&lt;P&gt;LPC_GPIO_PORT-&amp;gt;DIRSET[0] = (1 &amp;lt;&amp;lt; AVDD_ON);&lt;/P&gt;&lt;P&gt;AVDD_ON is equated to the port bit number.&lt;/P&gt;&lt;P&gt;I changed that to&lt;/P&gt;&lt;P&gt;LPC_GPIO_PORT-&amp;gt;DIRSET[0] = (1 &amp;lt;&amp;lt; AVDD_ON) || (1 &amp;lt;&amp;lt; PIO_4);&lt;/P&gt;&lt;P&gt;where PIO_4 is equated to 4.&lt;/P&gt;&lt;P&gt;It was one bar too much. It should have been bitwise or, not logical or.&lt;/P&gt;&lt;P&gt;Correct statement is&lt;/P&gt;&lt;P&gt;LPC_GPIO_PORT-&amp;gt;DIRSET[0] = (1 &amp;lt;&amp;lt; AVDD_ON) | (1 &amp;lt;&amp;lt; PIO_4);&lt;/P&gt;&lt;P&gt;And then it works.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2019 07:32:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869302#M34637</guid>
      <dc:creator>kurtmirdell</dc:creator>
      <dc:date>2019-04-01T07:32:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869303#M34638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;SPAN&gt;Hi&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class="" style="border: 0px;"&gt;&lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="284524" data-objecttype="3" href="https://community.nxp.com/people/kurtmirdell" style="color: #3d9ce7; background-color: transparent; border: 0px; font-weight: inherit; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;Kurt Mirdell&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Glad to hear the news.&lt;/P&gt;&lt;P style="border: 0px;"&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="border: 0px;"&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="border: 0px;"&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2019 11:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869303#M34638</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-04-01T11:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: LPC82X PIO0_4 as output</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869304#M34639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for sharing.&lt;/P&gt;&lt;P&gt;This has happened to me before, I looked at it for hours and didn't see it.&lt;/P&gt;&lt;P&gt;One thing that helps, when you are sufficiently desperate, is to look at the generated assembly code.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2019 12:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC82X-PIO0-4-as-output/m-p/869304#M34639</guid>
      <dc:creator>starblue</dc:creator>
      <dc:date>2019-04-01T12:21:26Z</dc:date>
    </item>
  </channel>
</rss>