<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Maximum Input Frequency of LPC81x? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-Input-Frequency-of-LPC81x/m-p/867953#M34595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to make a high frequency counter out of an LPC81x. I can use an external crystal to make the LPC81x run at 24 MHz, but I'd like to count&amp;nbsp;the frequencies of square waves in the 100MHz-200MHz range. Can I configure the SCT and its prescalers to count faster than the bus clock, or do I need to use a clock divider chip external to the LPC81x?&amp;nbsp;I cannot find the dynamic characteristics of the microcontroller's inputs in either the UM10601 LPC81x User Manual or the LPC81x datasheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jan 2019 15:21:29 GMT</pubDate>
    <dc:creator>tiberiumcode</dc:creator>
    <dc:date>2019-01-10T15:21:29Z</dc:date>
    <item>
      <title>Maximum Input Frequency of LPC81x?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-Input-Frequency-of-LPC81x/m-p/867953#M34595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to make a high frequency counter out of an LPC81x. I can use an external crystal to make the LPC81x run at 24 MHz, but I'd like to count&amp;nbsp;the frequencies of square waves in the 100MHz-200MHz range. Can I configure the SCT and its prescalers to count faster than the bus clock, or do I need to use a clock divider chip external to the LPC81x?&amp;nbsp;I cannot find the dynamic characteristics of the microcontroller's inputs in either the UM10601 LPC81x User Manual or the LPC81x datasheet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 15:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-Input-Frequency-of-LPC81x/m-p/867953#M34595</guid>
      <dc:creator>tiberiumcode</dc:creator>
      <dc:date>2019-01-10T15:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum Input Frequency of LPC81x?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-Input-Frequency-of-LPC81x/m-p/867954#M34596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="333770" data-username="tiberiumcode" href="https://community.nxp.com/people/tiberiumcode"&gt;Daniel Vibbert&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;Actually, the duration of the high and low levels on the input pin must be greater than 1 clock cycle, and the frequency of the input must be less than one-quarter of the clock rate.&lt;BR /&gt;About your question, the LPC81x is incapable of detecting the input PWM whose frequency exceeds the 100 MHz.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Jan 2019 03:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Maximum-Input-Frequency-of-LPC81x/m-p/867954#M34596</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-11T03:28:47Z</dc:date>
    </item>
  </channel>
</rss>