<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Can I only use the M0 core with LPC54114?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-only-use-the-M0-core-with-LPC54114/m-p/867063#M34571</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC5411x is intended for the M4 to release the M0+ since the M0+ is primarily there as a slave core, so the examples are geared up for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are looking for an M0+ only device with the same / very similar peripherals I'd suggest using the LPC51U68, which is a lower cost.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 09 Mar 2019 00:20:32 GMT</pubDate>
    <dc:creator>brendonslade</dc:creator>
    <dc:date>2019-03-09T00:20:32Z</dc:date>
    <item>
      <title>Can I only use the M0 core with LPC54114?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-only-use-the-M0-core-with-LPC54114/m-p/867062#M34570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found many examples about how to use dual cores. But no one said how to only use the M0 core to work. Is this possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Mar 2019 08:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-only-use-the-M0-core-with-LPC54114/m-p/867062#M34570</guid>
      <dc:creator>da_chen</dc:creator>
      <dc:date>2019-03-05T08:08:12Z</dc:date>
    </item>
    <item>
      <title>Re: Can I only use the M0 core with LPC54114?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-only-use-the-M0-core-with-LPC54114/m-p/867063#M34571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The LPC5411x is intended for the M4 to release the M0+ since the M0+ is primarily there as a slave core, so the examples are geared up for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are looking for an M0+ only device with the same / very similar peripherals I'd suggest using the LPC51U68, which is a lower cost.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 Mar 2019 00:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-I-only-use-the-M0-core-with-LPC54114/m-p/867063#M34571</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2019-03-09T00:20:32Z</dc:date>
    </item>
  </channel>
</rss>