<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC2478FBD208,551/Over Current Sense pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866963#M34569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello CarlosCasillas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the Input.&lt;/P&gt;&lt;P&gt;But here little bit confusion and not received my answer from the link suggested by you. So need further help from your side. I have Explained the Query as below. Please go through and provide your suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"I am using LPC2478FBD208,551 in my Product and now I am going to revise the Design. In previously I am using LCD Interface and 1 USB Host Interface and this design work very well. Now in new revision I want to add 1 more USB Host means 1 LCD+ 2 USB Host. The problem is that there are two pins which are shared between USB and LCD interface, Pin#88 (LCDVD[21]/USB_OVRCR1/) and Pin#74 (LCDVD[12]/USB_PWRD1/). &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;How can I use the 2 USB Host and 1 LCD at same time?"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So Please Guide to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alpesh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jan 2019 04:40:03 GMT</pubDate>
    <dc:creator>alpesh_borad</dc:creator>
    <dc:date>2019-01-30T04:40:03Z</dc:date>
    <item>
      <title>LPC2478FBD208,551/Over Current Sense pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866961#M34567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;LPC2478FBD208,551 in my project. Here I am going to use 2 USB type A and LCD Interface.&lt;/P&gt;&lt;P&gt;For Both the USB Type A i am using USB Over Current Sense IC which send OCE Signal to&amp;nbsp;LPC2478FBD208,551 for both the USB.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now the Pin#88 is shared between LCDVD14 and USB_OVRCR1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So my question is How to sense the OVRCR1 pin?&lt;/P&gt;&lt;P&gt;Can I use any GPIO Pin for the same?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest the Guidance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alpesh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 09:21:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866961#M34567</guid>
      <dc:creator>alpesh_borad</dc:creator>
      <dc:date>2019-01-28T09:21:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2478FBD208,551/Over Current Sense pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866962#M34568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alpesh,&lt;BR /&gt;You might add external over-current protection circuitry on USB ports. You could also take a look to the following link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.embeddedrelated.com/showthread/lpc2000/47524-1.php" title="https://www.embeddedrelated.com/showthread/lpc2000/47524-1.php"&gt;lpc2000 | LPC2478 with two USB host and LCD?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 01:07:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866962#M34568</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-01-29T01:07:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2478FBD208,551/Over Current Sense pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866963#M34569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello CarlosCasillas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the Input.&lt;/P&gt;&lt;P&gt;But here little bit confusion and not received my answer from the link suggested by you. So need further help from your side. I have Explained the Query as below. Please go through and provide your suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"I am using LPC2478FBD208,551 in my Product and now I am going to revise the Design. In previously I am using LCD Interface and 1 USB Host Interface and this design work very well. Now in new revision I want to add 1 more USB Host means 1 LCD+ 2 USB Host. The problem is that there are two pins which are shared between USB and LCD interface, Pin#88 (LCDVD[21]/USB_OVRCR1/) and Pin#74 (LCDVD[12]/USB_PWRD1/). &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;How can I use the 2 USB Host and 1 LCD at same time?"&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So Please Guide to me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Alpesh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2019 04:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC2478FBD208-551-Over-Current-Sense-pin/m-p/866963#M34569</guid>
      <dc:creator>alpesh_borad</dc:creator>
      <dc:date>2019-01-30T04:40:03Z</dc:date>
    </item>
  </channel>
</rss>