<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with LCD peripherals ( No LCD_ENAB_M) [ SOLVED ] in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LCD-peripherals-No-LCD-ENAB-M-SOLVED/m-p/520024#M3456</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leform14 on Tue Jan 13 06:07:11 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to use a TFT-panel with a lpc1788. I use as reference the source code for MOD-LCD.4.3"+ evaluation board. My config are good, I see my DOTCLK at the good speed but I can't see anything on the pin 2.4 (LCD_Enable_m). The mux register is set to FUNC_7, TFT and other parameters are ok but nothing appears on my screen except ugly bar of any color. I set a buffer of y lines and x pixels that I used as UpperPanel Frame base (single mode) but nothing ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anybody can help me to do a check of what I have done or give me tips please ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:41:44 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:41:44Z</dc:date>
    <item>
      <title>Problem with LCD peripherals ( No LCD_ENAB_M) [ SOLVED ]</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LCD-peripherals-No-LCD-ENAB-M-SOLVED/m-p/520024#M3456</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leform14 on Tue Jan 13 06:07:11 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I try to use a TFT-panel with a lpc1788. I use as reference the source code for MOD-LCD.4.3"+ evaluation board. My config are good, I see my DOTCLK at the good speed but I can't see anything on the pin 2.4 (LCD_Enable_m). The mux register is set to FUNC_7, TFT and other parameters are ok but nothing appears on my screen except ugly bar of any color. I set a buffer of y lines and x pixels that I used as UpperPanel Frame base (single mode) but nothing ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Anybody can help me to do a check of what I have done or give me tips please ?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:41:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LCD-peripherals-No-LCD-ENAB-M-SOLVED/m-p/520024#M3456</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:41:44Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with LCD peripherals ( No LCD_ENAB_M) [ SOLVED ]</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LCD-peripherals-No-LCD-ENAB-M-SOLVED/m-p/520025#M3457</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leform14 on Wed Jan 14 03:44:36 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;HI all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I solved my problem, that was due to the buffer (I use now 0x20000000). So now, I am able to use the mod-LCD.4.3"+ board with a code based on FreeRTOS/lpcOpen library (draw/cursor) and external SDRAM (buffer is now Dynamic memory chip select X address).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:41:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-with-LCD-peripherals-No-LCD-ENAB-M-SOLVED/m-p/520025#M3457</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:41:45Z</dc:date>
    </item>
  </channel>
</rss>