<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: unused pins , output-mode disable pull-down?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866743#M34555</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jun&lt;/P&gt;&lt;P&gt;Make the unused pin as floating, and then set it as output low in software. GPIO output with pull-up disabled, and pull-down enabled.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Mar 2019 09:02:04 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2019-03-19T09:02:04Z</dc:date>
    <item>
      <title>unused pins , output-mode disable pull-down?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866742#M34554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;BR /&gt;In the LPC82X data sheet, it is recommended to disable unused pins and output LOW in the output mode, but is it also possible to disable pull-down?&lt;BR /&gt;The MODE bit in the IOCON register is&lt;BR /&gt;0x0 Inactive (no pull-down / pull-up resistor enabled).&lt;BR /&gt;0x1 Pull-down resistor enabled.&lt;BR /&gt;0x2 Pull-up resistor enabled.&lt;BR /&gt;0x3 Repeater&lt;BR /&gt;So, which one is recommended, 0x0 or 0x01?&lt;BR /&gt;Sorry, I do not have much knowledge of hardware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 00:26:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866742#M34554</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-03-19T00:26:24Z</dc:date>
    </item>
    <item>
      <title>Re: unused pins , output-mode disable pull-down?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866743#M34555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jun&lt;/P&gt;&lt;P&gt;Make the unused pin as floating, and then set it as output low in software. GPIO output with pull-up disabled, and pull-down enabled.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 09:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866743#M34555</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-03-19T09:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: unused pins , output-mode disable pull-down?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866744#M34556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for a polite answer.&lt;BR /&gt;I understand that.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;jun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Mar 2019 23:26:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866744#M34556</guid>
      <dc:creator>jun1</dc:creator>
      <dc:date>2019-03-19T23:26:27Z</dc:date>
    </item>
    <item>
      <title>Re: unused pins , output-mode disable pull-down?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866745#M34557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You are welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Mar 2019 02:27:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/unused-pins-output-mode-disable-pull-down/m-p/866745#M34557</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-03-20T02:27:36Z</dc:date>
    </item>
  </channel>
</rss>