<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Resetting LPC546xx while writing to external static RAM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866294#M34540</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ref. LPC546xx datasheet fig.25 External static memory read/write access&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does a&amp;nbsp;low on the reset pin abort an external write cycle -&amp;nbsp;if going low in the WR5 window - with&amp;nbsp;a chance for leaving&amp;nbsp;garbage in the addressed SRAM location?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or will the reset action be delayed until the writecycle has finished?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just short -&amp;nbsp;is the action of a low reset asynchronous or synchronous with what the CPU is actually doing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Viggo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Feb 2019 13:09:46 GMT</pubDate>
    <dc:creator>vijo</dc:creator>
    <dc:date>2019-02-15T13:09:46Z</dc:date>
    <item>
      <title>Resetting LPC546xx while writing to external static RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866294#M34540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ref. LPC546xx datasheet fig.25 External static memory read/write access&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does a&amp;nbsp;low on the reset pin abort an external write cycle -&amp;nbsp;if going low in the WR5 window - with&amp;nbsp;a chance for leaving&amp;nbsp;garbage in the addressed SRAM location?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or will the reset action be delayed until the writecycle has finished?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just short -&amp;nbsp;is the action of a low reset asynchronous or synchronous with what the CPU is actually doing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Viggo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 13:09:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866294#M34540</guid>
      <dc:creator>vijo</dc:creator>
      <dc:date>2019-02-15T13:09:46Z</dc:date>
    </item>
    <item>
      <title>Re: Resetting LPC546xx while writing to external static RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866295#M34541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Viggo,&lt;/P&gt;&lt;P&gt;If you clear the EMCSYSCTRL[EMCRD] bit, both the POR RESET event and the Reset Pin/Watchdog Reset events can reset the EMC module.&lt;/P&gt;&lt;P&gt;If you set the EMCSYSCTRL[EMCRD] bit, only the POR RESET event can reset the EMC module, The Reset pin/Watchdog reset events can not reset the EMC module in the condition.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Once the EMC module is reset, all registers and functions of the EMC are initialized to it's Reset states immediately, in other words, the Reset event is asynchronous with the CPU action.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 08:07:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866295#M34541</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-02-18T08:07:36Z</dc:date>
    </item>
    <item>
      <title>Re: Resetting LPC546xx while writing to external static RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866296#M34542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for the information TIC,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;will a reset of the EMC module immediately abort a memory write cycle to a external SRAM ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Viggo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Feb 2019 09:20:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866296#M34542</guid>
      <dc:creator>vijo</dc:creator>
      <dc:date>2019-02-18T09:20:09Z</dc:date>
    </item>
    <item>
      <title>Re: Resetting LPC546xx while writing to external static RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866297#M34543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Viggo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, a reset event of the EMC module immediately aborts a memory write cycle to a external SRAM.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Feb 2019 06:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Resetting-LPC546xx-while-writing-to-external-static-RAM/m-p/866297#M34543</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-02-19T06:53:17Z</dc:date>
    </item>
  </channel>
</rss>