<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 About LPC844 I2C question</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC844-I2C-question/m-p/865465#M34508</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, All,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I used the LPC844 I2C module in slave mode. But the another MCU works very faster than LPC844. So, I need that LPC844 could hold SCL clock line low after a complete I2C transmission, indicating that it is busy now. After LPC844 complete the current process, LPC844 release SCL single, then the main MCU could operate I2C bus normally.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I do not find this function in user manual. How to realize these I2C operation in software?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Hope to help to settle my question. Thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Jan 2019 04:25:44 GMT</pubDate>
    <dc:creator>DerekXiang</dc:creator>
    <dc:date>2019-01-10T04:25:44Z</dc:date>
    <item>
      <title>About LPC844 I2C question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC844-I2C-question/m-p/865465#M34508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, All,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I used the LPC844 I2C module in slave mode. But the another MCU works very faster than LPC844. So, I need that LPC844 could hold SCL clock line low after a complete I2C transmission, indicating that it is busy now. After LPC844 complete the current process, LPC844 release SCL single, then the main MCU could operate I2C bus normally.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;I do not find this function in user manual. How to realize these I2C operation in software?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Hope to help to settle my question. Thanks!!!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jan 2019 04:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC844-I2C-question/m-p/865465#M34508</guid>
      <dc:creator>DerekXiang</dc:creator>
      <dc:date>2019-01-10T04:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: About LPC844 I2C question</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC844-I2C-question/m-p/865466#M34509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When the LPC844 works in slave mode, the slave IIC module is not able to drive the SCL low to have a delay between two transfer after the completion of current data transfer.&lt;/P&gt;&lt;P&gt;I think you can have master&amp;nbsp; add a delay between the data transfer so that the slave has enough time to handle the data reading/writting.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 05:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/About-LPC844-I2C-question/m-p/865466#M34509</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-01-16T05:15:07Z</dc:date>
    </item>
  </channel>
</rss>