<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMRT has only 24 bit</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRT-has-only-24-bit/m-p/513774#M344</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ER-Berlin on Thu Feb 27 05:44:20 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I love the simple to use MRT-Timer on the LPC8xx controller. I was happy to read that this timers are also implemented in the new LPC15xx controllers. But WHY are the timer registers only 24 bit wide? With a 72 MHz system clock the longest timeout possible is only 233 ms. This is too short for most applications, e.g. serial receive timeout. Now i have to learn the use of SCT for longer timeouts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Greetings from germany, Erwin&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:10:41 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:10:41Z</dc:date>
    <item>
      <title>MRT has only 24 bit</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRT-has-only-24-bit/m-p/513774#M344</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ER-Berlin on Thu Feb 27 05:44:20 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I love the simple to use MRT-Timer on the LPC8xx controller. I was happy to read that this timers are also implemented in the new LPC15xx controllers. But WHY are the timer registers only 24 bit wide? With a 72 MHz system clock the longest timeout possible is only 233 ms. This is too short for most applications, e.g. serial receive timeout. Now i have to learn the use of SCT for longer timeouts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Greetings from germany, Erwin&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MRT-has-only-24-bit/m-p/513774#M344</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: MRT has only 24 bit</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MRT-has-only-24-bit/m-p/513775#M345</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by R2D2 on Thu Feb 27 06:53:35 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: ER-Berlin&lt;/STRONG&gt;&lt;BR /&gt;...longer timeouts.&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;And the winner is...................RIT&amp;nbsp; :O &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Chapter 20: LPC15xx Repetitive Interrupt Timer (RIT)&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;20.2 Features&lt;BR /&gt;• [color=#f00]48-bit[/color] counter&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Perhaps your lost bits are there?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MRT-has-only-24-bit/m-p/513775#M345</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:10:41Z</dc:date>
    </item>
  </channel>
</rss>