<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ISP over RS-485? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-RS-485/m-p/513770#M343</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdupre on Thu Aug 13 21:56:04 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No comment?&amp;nbsp; Is it impossible for the ISP ROM &amp;amp; hardware in the LPC15xx to signal TxEnable for an RS-485 transceiver?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looks like I can do it with IAP, but it sure would be better to have this possible with the ISP interface.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:08:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:08:57Z</dc:date>
    <item>
      <title>ISP over RS-485?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-RS-485/m-p/513769#M342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdupre on Tue Aug 04 12:56:47 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Is it possible to use ISP mode at boot if an RS-485 transceiver is on the ISP UART?&amp;nbsp; If so, how does one control the direction (TxEnable) so an autobaud response can be sent?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC2xxx has a means to control this via the reset and ISP entry pins.&amp;nbsp; But the LPC15xx has two ISP entry pins and I find no mention of the ISP code being able to control RTS in the manual.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;- Joe&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:08:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-RS-485/m-p/513769#M342</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:08:56Z</dc:date>
    </item>
    <item>
      <title>Re: ISP over RS-485?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-RS-485/m-p/513770#M343</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jdupre on Thu Aug 13 21:56:04 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;No comment?&amp;nbsp; Is it impossible for the ISP ROM &amp;amp; hardware in the LPC15xx to signal TxEnable for an RS-485 transceiver?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Looks like I can do it with IAP, but it sure would be better to have this possible with the ISP interface.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ISP-over-RS-485/m-p/513770#M343</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:08:57Z</dc:date>
    </item>
  </channel>
</rss>