<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: lpc1756 vbat UL Certification</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1756-vbat-UL-Certification/m-p/860676#M34254</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the LPC1768 with VBAT connected to CR2032 and I just had the same questions coming from CSA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone from NXP provide&amp;nbsp;us with some more information about the power selector block as shown in the UM10360 user manual Figure 131? I've copied the block diagram below for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there internal blocking diodes and current limit resistors to prevent current from VDD(REG)(3v3) to VBAT and vice versa?&amp;nbsp;If there is&amp;nbsp;3.3V present on VDD(REG)(3v3), will there be reverse charge current flowing out of VBAT?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78831i4F9E96B987EF1A70/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is&amp;nbsp;the circuit below implemented internally in the Power selector block, or does that need to be implemented externally?&lt;/P&gt;&lt;P&gt;If there is another equivalent circuit internally, what is the circuit? (to satisfy&amp;nbsp;safety certification questions).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79106i6C3CD87ECFCAB98A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Mar 2019 20:35:40 GMT</pubDate>
    <dc:creator>udellso</dc:creator>
    <dc:date>2019-03-28T20:35:40Z</dc:date>
    <item>
      <title>lpc1756 vbat UL Certification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1756-vbat-UL-Certification/m-p/860675#M34253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have connected a CR2032 to VBAT of the LPC1756 and it seems like there are questions regarding the protection of the battery against charging currents from the UL certification. Has anyone been in the same situation? Is it useful to know the implemented circuit of VBAT pin of LPC1756?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2019 07:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1756-vbat-UL-Certification/m-p/860675#M34253</guid>
      <dc:creator>quyentran</dc:creator>
      <dc:date>2019-03-01T07:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: lpc1756 vbat UL Certification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1756-vbat-UL-Certification/m-p/860676#M34254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the LPC1768 with VBAT connected to CR2032 and I just had the same questions coming from CSA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone from NXP provide&amp;nbsp;us with some more information about the power selector block as shown in the UM10360 user manual Figure 131? I've copied the block diagram below for reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there internal blocking diodes and current limit resistors to prevent current from VDD(REG)(3v3) to VBAT and vice versa?&amp;nbsp;If there is&amp;nbsp;3.3V present on VDD(REG)(3v3), will there be reverse charge current flowing out of VBAT?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/78831i4F9E96B987EF1A70/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is&amp;nbsp;the circuit below implemented internally in the Power selector block, or does that need to be implemented externally?&lt;/P&gt;&lt;P&gt;If there is another equivalent circuit internally, what is the circuit? (to satisfy&amp;nbsp;safety certification questions).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79106i6C3CD87ECFCAB98A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Mar 2019 20:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc1756-vbat-UL-Certification/m-p/860676#M34254</guid>
      <dc:creator>udellso</dc:creator>
      <dc:date>2019-03-28T20:35:40Z</dc:date>
    </item>
  </channel>
</rss>