<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC546XX User Guide and CAN Bus Info.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-User-Guide-and-CAN-Bus-Info/m-p/859347#M34210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the LPC564xx User Manual UM10912 Rev 2.2 for some CAN info. Right now I'm trying to figure out the TX FIFO, queue and dedicated buffer relationship and have a problem with the documentation. To me it seems that sections 35.14.7.3 Tx FIFO and 35.14.7.4 Tx queue on page 756 aren't correct and some of the info in the Tx FIFO section is for the Tx queue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;35.14.7.3 Tx FIFO&lt;BR /&gt;Tx queue operation is configured by setting the TFQM bit in the TXBC register. Messages&lt;BR /&gt;stored in the Tx queue are transmitted starting with the message with the lowest message&lt;BR /&gt;ID (highest priority). In case multiple queue buffers are configured with the same message&lt;BR /&gt;ID, the queue buffer with the lowest buffer number is transmitted first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;35.14.7.4 Tx queue&lt;BR /&gt;Tx queue operation is configured by programming the TFQM bit field to a value of one.&lt;BR /&gt;Messages stored in the Tx queue are transmitted starting with the message with the&lt;BR /&gt;lowest message ID (highest priority). In case that multiple queue buffers are configured&lt;BR /&gt;with the same message ID, the queue buffer with the lowest buffer number is transmitted&lt;BR /&gt;first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an updated user manual or a better on line reference for the LP546XX CAN interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Jay S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Feb 2019 19:15:15 GMT</pubDate>
    <dc:creator>jays</dc:creator>
    <dc:date>2019-02-28T19:15:15Z</dc:date>
    <item>
      <title>LPC546XX User Guide and CAN Bus Info.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-User-Guide-and-CAN-Bus-Info/m-p/859347#M34210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the LPC564xx User Manual UM10912 Rev 2.2 for some CAN info. Right now I'm trying to figure out the TX FIFO, queue and dedicated buffer relationship and have a problem with the documentation. To me it seems that sections 35.14.7.3 Tx FIFO and 35.14.7.4 Tx queue on page 756 aren't correct and some of the info in the Tx FIFO section is for the Tx queue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;35.14.7.3 Tx FIFO&lt;BR /&gt;Tx queue operation is configured by setting the TFQM bit in the TXBC register. Messages&lt;BR /&gt;stored in the Tx queue are transmitted starting with the message with the lowest message&lt;BR /&gt;ID (highest priority). In case multiple queue buffers are configured with the same message&lt;BR /&gt;ID, the queue buffer with the lowest buffer number is transmitted first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;35.14.7.4 Tx queue&lt;BR /&gt;Tx queue operation is configured by programming the TFQM bit field to a value of one.&lt;BR /&gt;Messages stored in the Tx queue are transmitted starting with the message with the&lt;BR /&gt;lowest message ID (highest priority). In case that multiple queue buffers are configured&lt;BR /&gt;with the same message ID, the queue buffer with the lowest buffer number is transmitted&lt;BR /&gt;first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an updated user manual or a better on line reference for the LP546XX CAN interface?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Jay S.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Feb 2019 19:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-User-Guide-and-CAN-Bus-Info/m-p/859347#M34210</guid>
      <dc:creator>jays</dc:creator>
      <dc:date>2019-02-28T19:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546XX User Guide and CAN Bus Info.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-User-Guide-and-CAN-Bus-Info/m-p/859348#M34211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="335684" data-username="jays@versalogic.com" href="https://community.nxp.com/people/jays@versalogic.com"&gt;Jay Schwichtenberg.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your sharing, I have reported this to development team, they said will fix it next version.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Mar 2019 07:08:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546XX-User-Guide-and-CAN-Bus-Info/m-p/859348#M34211</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-03-11T07:08:33Z</dc:date>
    </item>
  </channel>
</rss>