<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Two image(frimware) on LPC1830 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Two-image-frimware-on-LPC1830/m-p/858755#M34186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I need run two firmware with LPC1830, and the compiler is use MCUXpresso,&lt;/P&gt;&lt;P&gt;After I jump to second image, is it possible that I can still use step by step to debug with LPC Link?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For first image, it can use step by step on MCUXpresso, after I copy second image to another ram(Ex: SDRAM) by image1.&lt;/P&gt;&lt;P&gt;I want to know if I can debug with step by step?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My flow will be like:&lt;/P&gt;&lt;P&gt;Image1: Run some application and copy image2 from Flash to SDRAM and jump to image2.&lt;/P&gt;&lt;P&gt;iamge2: Run second application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jan 2019 10:25:35 GMT</pubDate>
    <dc:creator>kensu</dc:creator>
    <dc:date>2019-01-24T10:25:35Z</dc:date>
    <item>
      <title>Two image(frimware) on LPC1830</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Two-image-frimware-on-LPC1830/m-p/858755#M34186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dears&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I need run two firmware with LPC1830, and the compiler is use MCUXpresso,&lt;/P&gt;&lt;P&gt;After I jump to second image, is it possible that I can still use step by step to debug with LPC Link?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For first image, it can use step by step on MCUXpresso, after I copy second image to another ram(Ex: SDRAM) by image1.&lt;/P&gt;&lt;P&gt;I want to know if I can debug with step by step?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My flow will be like:&lt;/P&gt;&lt;P&gt;Image1: Run some application and copy image2 from Flash to SDRAM and jump to image2.&lt;/P&gt;&lt;P&gt;iamge2: Run second application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 10:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Two-image-frimware-on-LPC1830/m-p/858755#M34186</guid>
      <dc:creator>kensu</dc:creator>
      <dc:date>2019-01-24T10:25:35Z</dc:date>
    </item>
    <item>
      <title>Re: Two image(frimware) on LPC1830</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Two-image-frimware-on-LPC1830/m-p/858756#M34187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="293120" data-username="kensu" href="https://community.nxp.com/people/kensu"&gt;Ken Su&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) After I jump to the second image, is it possible that I can still use step by step to debug with LPC Link?&lt;BR /&gt;-- No, I'm afraid not.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2019 01:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Two-image-frimware-on-LPC1830/m-p/858756#M34187</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-25T01:59:04Z</dc:date>
    </item>
  </channel>
</rss>