<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Lpc845 app code can't debug after bootloader</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856991#M34084</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My operation flow situation,&lt;/P&gt;&lt;P&gt;burning my boootloader program at address 0x0~0x2CFF. Then, burning the application program at address 0x3000~(size 0xb000). Where burn the application program by LPCLinkII and debug in MCUXpresso.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general, when I burn the application code&amp;nbsp;&lt;SPAN&gt;by LPCLinkII, it should startup from the bootloader(0x0) and jump to the application code(0x3000) and stop at the first line of the main() function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So,&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If I do not use the SPI interrupt in the bootloader code, it works, it correct jump from bootloader to application main().&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f; "&gt;But, If I use the SPI interrupt in the bootloader code,&amp;nbsp;&amp;nbsp;it doesn't jump&amp;nbsp;from bootloader to application main().&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I used the method several MCUs, but&amp;nbsp;I usually use UART in bootloader code, it's my first time use the SPI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used the method with LPC824, but I used the uart in bootloader coed, not spi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Feb 2019 03:45:19 GMT</pubDate>
    <dc:creator>lojyunmin</dc:creator>
    <dc:date>2019-02-13T03:45:19Z</dc:date>
    <item>
      <title>Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856989#M34082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a problem, my application code can't correct run in debug mode with MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;I used SPI interrupt in my bootloader.&lt;/P&gt;&lt;P&gt;Then, my App code work correct without debug mode, but can't work correct in debug mode.&lt;/P&gt;&lt;P&gt;If I do not use the SPI interrupt, it can work correct in debug mode. Why?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I seem&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/494497"&gt;LPC845 Jumping to secondary Application&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/people/Alice_Yang" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: none; font-size: 1.286rem;"&gt;Alice_Yang&lt;/A&gt;&lt;SPAN style="color: #3d9ce7; background-color: #ffffff; font-weight: 500;"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="&amp;amp;#21729;&amp;amp;#24037;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/123549iFDB2632CE0F3284E/image-size/large?v=v2&amp;amp;px=999" role="button" title="&amp;amp;#21729;&amp;amp;#24037;" alt="&amp;amp;#21729;&amp;amp;#24037;" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;In default,&amp;nbsp; the MCUXpresso IDE can't debug application with start address from 0x3000( only can start from 0x0000).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"In default", are there any other settings missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 05:51:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856989#M34082</guid>
      <dc:creator>lojyunmin</dc:creator>
      <dc:date>2019-02-12T05:51:39Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856990#M34083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What do you actually mean by "my App code work correct without debug mode, but can't work correct in debug mode" ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With regards to "MCUXpresso IDE can't debug application with start address from 0x3000", after programming flash, the IDE will by default reset the device - which causes the ROM bootrom code to run and call into a"valid image" in flash at 0x0. Thus if you have no valid image&amp;nbsp;in flash at 0x0 this is not going to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One allow you to debug your application at 0x3000&amp;nbsp;via a LinkServer / CMSIS-DAP debug connection (assuming you have your boot loader or a "dummy application" at address 0x0) would probably be to change the way that the IDE resets the target after programming flash. To do this, edit the launch configuration (by double clicking on the .launch file that will have been created in your project) and change the "reset handling" option to "SOFT".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72023i52D2A9BFBF1DD821/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 19:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856990#M34083</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-02-12T19:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856991#M34084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My operation flow situation,&lt;/P&gt;&lt;P&gt;burning my boootloader program at address 0x0~0x2CFF. Then, burning the application program at address 0x3000~(size 0xb000). Where burn the application program by LPCLinkII and debug in MCUXpresso.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In general, when I burn the application code&amp;nbsp;&lt;SPAN&gt;by LPCLinkII, it should startup from the bootloader(0x0) and jump to the application code(0x3000) and stop at the first line of the main() function.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;So,&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;If I do not use the SPI interrupt in the bootloader code, it works, it correct jump from bootloader to application main().&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #51626f; "&gt;But, If I use the SPI interrupt in the bootloader code,&amp;nbsp;&amp;nbsp;it doesn't jump&amp;nbsp;from bootloader to application main().&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way, I used the method several MCUs, but&amp;nbsp;I usually use UART in bootloader code, it's my first time use the SPI.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I used the method with LPC824, but I used the uart in bootloader coed, not spi.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 03:45:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856991#M34084</guid>
      <dc:creator>lojyunmin</dc:creator>
      <dc:date>2019-02-13T03:45:19Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856992#M34085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I suspect the SPI interrupt handler (in the bootloader) is possibly not setting up the application reset context properly to vector to the application. Note the application startup initialized the VTOR to its own vector table. Until that happens, any active interrupts would vector back into the bootloader. Double check this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 04:21:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856992#M34085</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-02-13T04:21:02Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856993#M34086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;this is the function before jump&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;USER_ENTRY_PFN user_entry;&lt;BR /&gt; NVIC_DisableIRQ(BOD_IRQn); //Enable BOD IRQ&lt;BR /&gt; NVIC_DisableIRQ(SPI0_IRQn);&lt;BR /&gt; #if defined(WDT_ON)&lt;BR /&gt; NVIC_DisableIRQ(WDT_IRQn); //Disable Watch Dog IRQ&lt;BR /&gt; #endif&lt;BR /&gt; __disable_irq();&lt;BR /&gt; SCB-&amp;gt;VTOR = APP_CODE_START_ADDR;&lt;BR /&gt; user_entry = (USER_ENTRY_PFN)*((uint32_t*)(APP_CODE_START_ADDR + 4));&lt;/P&gt;&lt;P&gt;(user_entry)();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and this is the&amp;nbsp;interrupt function, it almost like the spi sample code&lt;/P&gt;&lt;P&gt;void SPI0_IRQHandler(void)&lt;BR /&gt;{&lt;BR /&gt; Chip_SPI_Int_Cmd(LPC_SPI0, SPI_INTENCLR_TXDYEN | SPI_INTENCLR_RXDYEN | SPI_INTENCLR_RXOVEN | SPI_INTENCLR_TXUREN, DISABLE);/* Disable all interrupt */&lt;BR /&gt; if (((gstXfSetup.pRx) &amp;amp;&amp;amp; (gstXfSetup.RxCnt &amp;lt; gstXfSetup.Length)) || ((gstXfSetup.pTx) &amp;amp;&amp;amp; (gstXfSetup.TxCnt &amp;lt; gstXfSetup.Length)))&lt;BR /&gt; {&lt;BR /&gt; Chip_SPI_Int_RWFrames(LPC_SPI0, &amp;amp;gstXfSetup);&lt;BR /&gt; Chip_SPI_Int_Cmd(LPC_SPI0, SPI_INTENSET_TXDYEN | SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN, ENABLE);&lt;BR /&gt; }&lt;BR /&gt; else &lt;BR /&gt; {&lt;BR /&gt; gbIsXferCompleted = true;&lt;BR /&gt; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and the spi read function, it reference lpc824&amp;nbsp;&lt;/P&gt;&lt;P&gt;void ReadSPIData(uint8_t aucDataLength) // length involve read cts byte&lt;BR /&gt;{&lt;BR /&gt; gbIsXferCompleted = false; //clear the flag&lt;BR /&gt; ConfigSPIStructure(aucDataLength);&lt;BR /&gt; Chip_SPI_Int_RWFrames(LPC_SPI0, &amp;amp;gstXfSetup);&lt;BR /&gt; Chip_SPI_Int_Cmd(LPC_SPI0, SPI_INTENSET_TXDYEN | SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN, ENABLE);&lt;BR /&gt; while (!gbIsXferCompleted) {}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I use&amp;nbsp;&lt;SPAN&gt;ReadSPIData() function, the jump is going to fail.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;any missing?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 05:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856993#M34086</guid>
      <dc:creator>lojyunmin</dc:creator>
      <dc:date>2019-02-13T05:28:07Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856994#M34087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This method solve my issue, but also let the application program work incorrect.&lt;/P&gt;&lt;P&gt;My application has open the optimize.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 07:02:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856994#M34087</guid>
      <dc:creator>lojyunmin</dc:creator>
      <dc:date>2019-02-13T07:02:35Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc845 app code can't debug after bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856995#M34088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I presume it's the bootloader using SPI? You didn't say how SPI is being used. Another possibility is the SYSMEMREMAP register is not setup as you expect. Set the launch configuration Reset Handling entry to SYSRESETREQ and report your results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;MCUXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Feb 2019 23:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc845-app-code-can-t-debug-after-bootloader/m-p/856995#M34088</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-02-13T23:44:32Z</dc:date>
    </item>
  </channel>
</rss>