<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic need to implement RS485 Slave on lpc in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/need-to-implement-RS485-Slave-on-lpc/m-p/855735#M34051</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to implement RS485 slave protocol on lpc1857 using UART3. Please inform if anyone has the code for the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want listen for the command from Arduino as a RS485 master and want lpc1857 to answer the command using RS485 slave.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Shruti P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Feb 2019 11:25:21 GMT</pubDate>
    <dc:creator>shruti_patel</dc:creator>
    <dc:date>2019-02-27T11:25:21Z</dc:date>
    <item>
      <title>need to implement RS485 Slave on lpc</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/need-to-implement-RS485-Slave-on-lpc/m-p/855735#M34051</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to implement RS485 slave protocol on lpc1857 using UART3. Please inform if anyone has the code for the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want listen for the command from Arduino as a RS485 master and want lpc1857 to answer the command using RS485 slave.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Shruti P&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Feb 2019 11:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/need-to-implement-RS485-Slave-on-lpc/m-p/855735#M34051</guid>
      <dc:creator>shruti_patel</dc:creator>
      <dc:date>2019-02-27T11:25:21Z</dc:date>
    </item>
  </channel>
</rss>