<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC51U68 generate sound in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-generate-sound/m-p/854651#M33991</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I use&amp;nbsp;LPC51U68 to generate sound? Is there guideline or sample code?&lt;/P&gt;&lt;P&gt;Is it possible to play speech recording file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Jan 2019 11:13:35 GMT</pubDate>
    <dc:creator>larry781111</dc:creator>
    <dc:date>2019-01-23T11:13:35Z</dc:date>
    <item>
      <title>LPC51U68 generate sound</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-generate-sound/m-p/854651#M33991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How can I use&amp;nbsp;LPC51U68 to generate sound? Is there guideline or sample code?&lt;/P&gt;&lt;P&gt;Is it possible to play speech recording file?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 11:13:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-generate-sound/m-p/854651#M33991</guid>
      <dc:creator>larry781111</dc:creator>
      <dc:date>2019-01-23T11:13:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPC51U68 generate sound</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-generate-sound/m-p/854652#M33992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="331037" data-username="larry781111@gmail.com" href="https://community.nxp.com/people/larry781111@gmail.com"&gt;YuChia Chien&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1） How can I use LPC51U68 to generate sound?&lt;BR /&gt;-- Yes, as the LPC51U68 has the I2S bus interface.&lt;BR /&gt;2) Is there a guideline or sample code?&lt;BR /&gt;-- Please refer the application note：&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11819.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11819.pdf&lt;/A&gt;&lt;BR /&gt;3） Is it possible to play speech recording file?&lt;BR /&gt;-- Of course, the MCU can receive the audio data from the USB, read the audio file in the SD, etc, then, play it via I2S transfer this data to the audio amplifier.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jan 2019 02:56:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC51U68-generate-sound/m-p/854652#M33992</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-24T02:56:06Z</dc:date>
    </item>
  </channel>
</rss>