<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: UM11029 Rev. 1.6 User Manual LPC84x: Errors in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854503#M33978</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="283988" data-username="1234567890" href="https://community.nxp.com/people/1234567890"&gt;12345 67890&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Thanks for your sharing,&amp;nbsp; I have checked them on User Manual.&lt;/P&gt;&lt;P&gt;I agree with you,&amp;nbsp; I have reported then to development team.&lt;/P&gt;&lt;P&gt;About page 38&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The maximum number of parameters is 5, passed to the "Copy RAM to FLASH" command.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The maximum number of results is 5, returned by the "ReadUID" command."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I think the " parameters 5 " included command (Copy RAM to FLASH), the "results is 5" includes&lt;/P&gt;&lt;P&gt;“state”, they are corresponding to the defined data structure when using IAP function:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72018i06867E31719948EC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 Feb 2019 03:08:51 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2019-02-12T03:08:51Z</dc:date>
    <item>
      <title>UM11029 Rev. 1.6 User Manual LPC84x: Errors</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854502#M33977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Table 13: As the LPC84x has 64 kB flash: Where in the table is the column for sector 32-63?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There seem to be typos (copy&amp;amp;paste from somewhere else) on page 38:&lt;/P&gt;&lt;P&gt;-The maximum number of parameters and results is 4, not 5.&lt;/P&gt;&lt;P&gt;- LPC84x is a M0+, not a M4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Feb 2019 17:56:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854502#M33977</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2019-02-11T17:56:09Z</dc:date>
    </item>
    <item>
      <title>Re: UM11029 Rev. 1.6 User Manual LPC84x: Errors</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854503#M33978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="283988" data-username="1234567890" href="https://community.nxp.com/people/1234567890"&gt;12345 67890&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Thanks for your sharing,&amp;nbsp; I have checked them on User Manual.&lt;/P&gt;&lt;P&gt;I agree with you,&amp;nbsp; I have reported then to development team.&lt;/P&gt;&lt;P&gt;About page 38&lt;/P&gt;&lt;P&gt;&lt;EM&gt;"The maximum number of parameters is 5, passed to the "Copy RAM to FLASH" command.&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;The maximum number of results is 5, returned by the "ReadUID" command."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I think the " parameters 5 " included command (Copy RAM to FLASH), the "results is 5" includes&lt;/P&gt;&lt;P&gt;“state”, they are corresponding to the defined data structure when using IAP function:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/72018i06867E31719948EC/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Feb 2019 03:08:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854503#M33978</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-02-12T03:08:51Z</dc:date>
    </item>
    <item>
      <title>Re: UM11029 Rev. 1.6 User Manual LPC84x: Errors</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854504#M33979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;- Table 123 says: CLKOUT function is coded in PINASSIGN 8, Table 189. Shouldn't it be PINASSIGN11, Table 192?&lt;/P&gt;&lt;P&gt;- Table 470, bit 16, value 0: Really 700 mA, not 700 µA???&lt;/P&gt;&lt;P&gt;- Page 359: "Clear the timer reset using the PRESETCTRL1 register (Table 150 for CTIMER)." It must be Table 149.&lt;/P&gt;&lt;P&gt;- Page 252: "The bits in the register not used for deep power-down control (bits 31:4) can be used for storing additional data..." Obviously bits 31:8 instead of 31:4.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 10:11:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UM11029-Rev-1-6-User-Manual-LPC84x-Errors/m-p/854504#M33979</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2019-04-04T10:11:20Z</dc:date>
    </item>
  </channel>
</rss>