<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC 546xx - Possible to keep GPIO State and Config during Reset? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-546xx-Possible-to-keep-GPIO-State-and-Config-during-Reset/m-p/853453#M33909</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I never test this before, but you can try to first put the Value of 1 into the GPIO and then configure it as input, this should avoid a little bit the Glitch, but in fact, it is going to be, since the PAD, it is changing.&amp;nbsp; Other advice would be adding a weak pullup, to see if this take the glitch out. If this is not I am afraid you are going to need another hardware solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 Mar 2019 01:14:01 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2019-03-14T01:14:01Z</dc:date>
    <item>
      <title>LPC 546xx - Possible to keep GPIO State and Config during Reset?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-546xx-Possible-to-keep-GPIO-State-and-Config-during-Reset/m-p/853452#M33908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using the LPC 54618 microcontroller in a system to power on/off other devices using the microcontrollers GPIO Pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To update the LPC we reset it. During reset the GPIO Pins reset to default settings(Input with Pull-Up resistor) like it is specified in the User Manual(UM10912).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some devices that need to stay powered on during reset are wired in a way that those devices stay powered on during reset but as soon as we re-enter the GPIO configuration the Output glitches and the connected device turns off. Even if we set the correct GPIO state right after or even before.&lt;/P&gt;&lt;P&gt;If we don't configure GPIO the device off course stays powered on but at some time we need to configure GPIO again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a way to completely keep the GPIO Configuration and State of the Outputs during and after reset?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or do we have to look for a hardware solution?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone can help. Tell me if you need further information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2019 10:05:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-546xx-Possible-to-keep-GPIO-State-and-Config-during-Reset/m-p/853452#M33908</guid>
      <dc:creator>kevingomes</dc:creator>
      <dc:date>2019-03-13T10:05:54Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 546xx - Possible to keep GPIO State and Config during Reset?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-546xx-Possible-to-keep-GPIO-State-and-Config-during-Reset/m-p/853453#M33909</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I never test this before, but you can try to first put the Value of 1 into the GPIO and then configure it as input, this should avoid a little bit the Glitch, but in fact, it is going to be, since the PAD, it is changing.&amp;nbsp; Other advice would be adding a weak pullup, to see if this take the glitch out. If this is not I am afraid you are going to need another hardware solution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 01:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-546xx-Possible-to-keep-GPIO-State-and-Config-during-Reset/m-p/853453#M33909</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-03-14T01:14:01Z</dc:date>
    </item>
  </channel>
</rss>