<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC11U37H µsdcard sample</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U37H-%C2%B5sdcard-sample/m-p/853355#M33906</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to develop a system based on the LPC11U37H microcontroller to log temperatures. So i was looking in the LPCOpen samles but was unable to find one who write and read data to/from the sdcard. I am using the OM13074 (LPCXpresso LPC11U37H v2 board). &lt;/P&gt;&lt;P&gt;The LPCOpen i use is version 2.03 (11/22/2013). This version is already more than 5 years old and i was wondering if NXP was able to release an updated version in which i can find a sample on how to use the µsdcard located on the board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 10 Feb 2019 15:41:08 GMT</pubDate>
    <dc:creator>sergedemaseneer</dc:creator>
    <dc:date>2019-02-10T15:41:08Z</dc:date>
    <item>
      <title>LPC11U37H µsdcard sample</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U37H-%C2%B5sdcard-sample/m-p/853355#M33906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need to develop a system based on the LPC11U37H microcontroller to log temperatures. So i was looking in the LPCOpen samles but was unable to find one who write and read data to/from the sdcard. I am using the OM13074 (LPCXpresso LPC11U37H v2 board). &lt;/P&gt;&lt;P&gt;The LPCOpen i use is version 2.03 (11/22/2013). This version is already more than 5 years old and i was wondering if NXP was able to release an updated version in which i can find a sample on how to use the µsdcard located on the board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Feb 2019 15:41:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U37H-%C2%B5sdcard-sample/m-p/853355#M33906</guid>
      <dc:creator>sergedemaseneer</dc:creator>
      <dc:date>2019-02-10T15:41:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11U37H µsdcard sample</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U37H-%C2%B5sdcard-sample/m-p/853356#M33907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately,&amp;nbsp;there is no example code for sdcard.&amp;nbsp;customer need to port the SPI SD card code by themselves, the official lpcopen code already provides the SPI driver.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please check the following thread as reference.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/437740"&gt;https://community.nxp.com/thread/437740&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sorry for any inconvenience that may cause,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sol&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Feb 2019 16:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U37H-%C2%B5sdcard-sample/m-p/853356#M33907</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-02-15T16:56:22Z</dc:date>
    </item>
  </channel>
</rss>