<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC546 SRAMX Uses</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-SRAMX-Uses/m-p/853134#M33903</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="232929" data-username="guitardenver" href="https://community.nxp.com/people/guitardenver"&gt;Matt Lang&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) What advantage would putting the program stack in SRAMX be? and what advantage would putting "common data" on the SRAMX be?&lt;BR /&gt;-- Instruction fetch and data access allow for 1 cycle CPU access, it's definitely faster than the main SRAM which connects the System clock.&lt;BR /&gt;2) Is this used specifically for the XIF with SPIFI?&lt;BR /&gt;-- No.&lt;BR /&gt;3)&amp;nbsp; I also read the SRAMX is cleared on startup, is this true? It is cleared by hardware on startup without the C environment startup code clearing it?&lt;BR /&gt;-- Yes.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Jan 2019 03:08:28 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2019-01-23T03:08:28Z</dc:date>
    <item>
      <title>LPC546 SRAMX Uses</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-SRAMX-Uses/m-p/853133#M33902</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am developing on the LPC54605 MCU and I am reading about the SRAMX. I was wondering what this is commonly used for? What benefits can this have?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Users Manual says:&lt;BR /&gt;"This RAM can be used, for example, as the location for the program stack, common data, or any other use where a&lt;BR /&gt;separate access away from the Main SRAM has an advantage."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) What advantage would putting the program stack in SRAMX be?&lt;/P&gt;&lt;P&gt;2) What advantage would putting "common data" on the SRAMX be?&lt;/P&gt;&lt;P&gt;3) The SRAMX is on the local busses I-CODE D-CODE. Does this mean it much faster to execute code from this SRAM than the other SRAM banks? Or is this used specifically for the XIF with SPIFI?&lt;/P&gt;&lt;P&gt;4) I also read the SRAMX is cleared on startup, is this true? It is cleared by hardware on startup without the C environment startup code clearing it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Matt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 15:07:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-SRAMX-Uses/m-p/853133#M33902</guid>
      <dc:creator>guitardenver</dc:creator>
      <dc:date>2019-01-22T15:07:29Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546 SRAMX Uses</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-SRAMX-Uses/m-p/853134#M33903</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="232929" data-username="guitardenver" href="https://community.nxp.com/people/guitardenver"&gt;Matt Lang&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) What advantage would putting the program stack in SRAMX be? and what advantage would putting "common data" on the SRAMX be?&lt;BR /&gt;-- Instruction fetch and data access allow for 1 cycle CPU access, it's definitely faster than the main SRAM which connects the System clock.&lt;BR /&gt;2) Is this used specifically for the XIF with SPIFI?&lt;BR /&gt;-- No.&lt;BR /&gt;3)&amp;nbsp; I also read the SRAMX is cleared on startup, is this true? It is cleared by hardware on startup without the C environment startup code clearing it?&lt;BR /&gt;-- Yes.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jan 2019 03:08:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546-SRAMX-Uses/m-p/853134#M33903</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-01-23T03:08:28Z</dc:date>
    </item>
  </channel>
</rss>