<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Hardware Peripheral Write using Address</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849270#M33800</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No I used a different method&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Jan 2019 10:28:14 GMT</pubDate>
    <dc:creator>athmesh_n</dc:creator>
    <dc:date>2019-01-07T10:28:14Z</dc:date>
    <item>
      <title>Hardware Peripheral Write using Address</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849268#M33798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on MODBUS protocol, where I have to write to pin using address given by master. Is it possible to write to a peripheral using peripheral address?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IDE: MCUXpresso&lt;/P&gt;&lt;P&gt;Controller : LPC1517&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Brief:&lt;/P&gt;&lt;P&gt;I would like to write to GPIO PIN PIO1_0, whose byte address is 0x1c000020. So, in order to make the pin high, should I write to address 0x1c000020? I tried using the following code:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;DIV&gt;&amp;nbsp;uint8_t volatile *gpio = (uint8_t *)0x1c000020;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;*gpio = 0x1;&lt;/DIV&gt;&lt;/BLOCKQUOTE&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Is it possible to do so?a&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Dec 2018 05:27:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849268#M33798</guid>
      <dc:creator>athmesh_n</dc:creator>
      <dc:date>2018-12-08T05:27:41Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware Peripheral Write using Address</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849269#M33799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="318969" data-username="athmesh.n" href="https://community.nxp.com/people/athmesh.n"&gt;ATHMESH NANDAKUMAR&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Yes, you can.&lt;/P&gt;&lt;P&gt;Do you have any problem when you using it ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Dec 2018 14:28:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849269#M33799</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-12-10T14:28:02Z</dc:date>
    </item>
    <item>
      <title>Re: Hardware Peripheral Write using Address</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849270#M33800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No I used a different method&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Jan 2019 10:28:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Hardware-Peripheral-Write-using-Address/m-p/849270#M33800</guid>
      <dc:creator>athmesh_n</dc:creator>
      <dc:date>2019-01-07T10:28:14Z</dc:date>
    </item>
  </channel>
</rss>