<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Can LPC802 IO support 5V voltage pull high</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC802-IO-support-5V-voltage-pull-high/m-p/849035#M33784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;It's necessary to need a level shift in this implementation, just in case.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Jul 2018 03:12:32 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2018-07-06T03:12:32Z</dc:date>
    <item>
      <title>Can LPC802 IO support 5V voltage pull high</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC802-IO-support-5V-voltage-pull-high/m-p/849034#M33783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Customer plan to use LPC802 to connect to an 5V CODEC via 5V pull up I2C.&lt;/P&gt;&lt;P&gt;Since LPC802/804 input can support max 5.4V voltage, can customer do so in HW without level shift?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Jul 2018 10:32:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC802-IO-support-5V-voltage-pull-high/m-p/849034#M33783</guid>
      <dc:creator>li-chinwang</dc:creator>
      <dc:date>2018-07-05T10:32:54Z</dc:date>
    </item>
    <item>
      <title>Re: Can LPC802 IO support 5V voltage pull high</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC802-IO-support-5V-voltage-pull-high/m-p/849035#M33784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;It's necessary to need a level shift in this implementation, just in case.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jul 2018 03:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-LPC802-IO-support-5V-voltage-pull-high/m-p/849035#M33784</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2018-07-06T03:12:32Z</dc:date>
    </item>
  </channel>
</rss>