<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Having Problem working on SPI...</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Having-Problem-working-on-SPI/m-p/845030#M33617</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Nisarg,&lt;/P&gt;&lt;P&gt;I copy part of the data sheet of CS5463, from the description, the VA+ is 5V, but the VD+ can be from 3.3V to 5V, I suggest you connect 3.3V power supply to VD+ pin, in this way, all digital logic will be 3.3V, it is easy for the the LPC1768 to interface with.&lt;/P&gt;&lt;P&gt;If you do want to connect VD+ to 5V power supply, I suppose that a transceiver chip is required, one side is 5V, another side is 3.3V.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63648iFAA3138E2870CE59/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Dec 2018 03:13:55 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-12-10T03:13:55Z</dc:date>
    <item>
      <title>Having Problem working on SPI...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Having-Problem-working-on-SPI/m-p/845029#M33616</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on LPC1768, Interfaced with CS5463.&lt;/P&gt;&lt;P&gt;Getting Clock and MOSI pulses of 3.3V even making it open drain, As of my knowledge CS5463 needs Pulses having 4.8V for High Logic, Alias I am getting to 3.3V only That is why my SPI is malfunctioning, Readings are not stable and even not precised..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So how can i get upto 5V pulses from SPI pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards Nisarg.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Dec 2018 06:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Having-Problem-working-on-SPI/m-p/845029#M33616</guid>
      <dc:creator>nisargnyk</dc:creator>
      <dc:date>2018-12-07T06:26:19Z</dc:date>
    </item>
    <item>
      <title>Re: Having Problem working on SPI...</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Having-Problem-working-on-SPI/m-p/845030#M33617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Nisarg,&lt;/P&gt;&lt;P&gt;I copy part of the data sheet of CS5463, from the description, the VA+ is 5V, but the VD+ can be from 3.3V to 5V, I suggest you connect 3.3V power supply to VD+ pin, in this way, all digital logic will be 3.3V, it is easy for the the LPC1768 to interface with.&lt;/P&gt;&lt;P&gt;If you do want to connect VD+ to 5V power supply, I suppose that a transceiver chip is required, one side is 5V, another side is 3.3V.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63648iFAA3138E2870CE59/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Dec 2018 03:13:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Having-Problem-working-on-SPI/m-p/845030#M33617</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-12-10T03:13:55Z</dc:date>
    </item>
  </channel>
</rss>