<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピック100MHz SCT?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/100MHz-SCT/m-p/844838#M33592</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the LPC15xx datasheet it says that the maximum CPU Frequency is 72MHz, and also that the maximum output frequency of the PLL is 100MHz.&lt;/P&gt;&lt;P&gt;Does that mean that I can run the SCT block at 100MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Aug 2018 13:37:36 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2018-08-30T13:37:36Z</dc:date>
    <item>
      <title>100MHz SCT?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/100MHz-SCT/m-p/844838#M33592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the LPC15xx datasheet it says that the maximum CPU Frequency is 72MHz, and also that the maximum output frequency of the PLL is 100MHz.&lt;/P&gt;&lt;P&gt;Does that mean that I can run the SCT block at 100MHz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Aug 2018 13:37:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/100MHz-SCT/m-p/844838#M33592</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2018-08-30T13:37:36Z</dc:date>
    </item>
    <item>
      <title>Re: 100MHz SCT?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/100MHz-SCT/m-p/844839#M33593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ian,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Yes, from the datasheet, we can know the PLL clock output frequency can up to 100Mhz, but in the SCT module, the SCT PLL don't up that 72Mhz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Because, the SCT register still clocked by the system clock, it is 72Mhz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; So, please configure the SCT PLL up to 72Mhz, the SCT PLL normally can input to the input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; We have an example to use the SCT PLL 72Mhz, then input it in the IN7, you can refer to that usage:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11538.zip" title="https://www.nxp.com/docs/en/application-note/AN11538.zip"&gt;https://www.nxp.com/docs/en/application-note/AN11538.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; AN11538.pdf page 12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kerry&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2018 06:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/100MHz-SCT/m-p/844839#M33593</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2018-08-31T06:53:59Z</dc:date>
    </item>
  </channel>
</rss>