<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC43S30 SPIFI1 Bug</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837922#M33391</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have a behavior similar to error LPC 43xx SPIFI.1 on a 43S30 Revision D device.&lt;/P&gt;&lt;P&gt;It occurs at cold start though.&lt;/P&gt;&lt;P&gt;The device is bootstrapped to boot from external&amp;nbsp;flash via SPIFI.&lt;/P&gt;&lt;P&gt;After&amp;nbsp;applying power the device is held in reset for 300ms by an external supply monitor.&lt;/P&gt;&lt;P&gt;When the reset is released there is no activity on any of the SPIFI pins, means no SPIFI boot attempt at all.&lt;/P&gt;&lt;P&gt;The device will then start to toggle P1_1 with 1 Hz for 1 minute and then happily and reliably boot from external flash to work stable&amp;nbsp;until the next power cycle.&lt;/P&gt;&lt;P&gt;We have a batch of devices that either always boot correctly or always have the one minute delay which is not acceptable for the application. All those are revision D and on identical boards.&lt;/P&gt;&lt;P&gt;SPIFI.1 is not mentioned in the 43Sxx errata at all. Is it present and on what revisions?&lt;/P&gt;&lt;P&gt;SPIFI.1 is not supposed to occur at cold start. Can it occur on cold start as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the attached screenshot.&lt;/P&gt;&lt;P&gt;Vcc yellow: analog&lt;/P&gt;&lt;P&gt;SPIFI_CLK: D0&lt;/P&gt;&lt;P&gt;SPIFI_MISO: D1&lt;/P&gt;&lt;P&gt;BOOT_SRC0: D2&lt;/P&gt;&lt;P&gt;/Reset: D3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions for workarounds welcome!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tobias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Sep 2018 11:36:11 GMT</pubDate>
    <dc:creator>tobiasmeyer</dc:creator>
    <dc:date>2018-09-18T11:36:11Z</dc:date>
    <item>
      <title>LPC43S30 SPIFI1 Bug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837922#M33391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have a behavior similar to error LPC 43xx SPIFI.1 on a 43S30 Revision D device.&lt;/P&gt;&lt;P&gt;It occurs at cold start though.&lt;/P&gt;&lt;P&gt;The device is bootstrapped to boot from external&amp;nbsp;flash via SPIFI.&lt;/P&gt;&lt;P&gt;After&amp;nbsp;applying power the device is held in reset for 300ms by an external supply monitor.&lt;/P&gt;&lt;P&gt;When the reset is released there is no activity on any of the SPIFI pins, means no SPIFI boot attempt at all.&lt;/P&gt;&lt;P&gt;The device will then start to toggle P1_1 with 1 Hz for 1 minute and then happily and reliably boot from external flash to work stable&amp;nbsp;until the next power cycle.&lt;/P&gt;&lt;P&gt;We have a batch of devices that either always boot correctly or always have the one minute delay which is not acceptable for the application. All those are revision D and on identical boards.&lt;/P&gt;&lt;P&gt;SPIFI.1 is not mentioned in the 43Sxx errata at all. Is it present and on what revisions?&lt;/P&gt;&lt;P&gt;SPIFI.1 is not supposed to occur at cold start. Can it occur on cold start as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the attached screenshot.&lt;/P&gt;&lt;P&gt;Vcc yellow: analog&lt;/P&gt;&lt;P&gt;SPIFI_CLK: D0&lt;/P&gt;&lt;P&gt;SPIFI_MISO: D1&lt;/P&gt;&lt;P&gt;BOOT_SRC0: D2&lt;/P&gt;&lt;P&gt;/Reset: D3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions for workarounds welcome!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tobias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 11:36:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837922#M33391</guid>
      <dc:creator>tobiasmeyer</dc:creator>
      <dc:date>2018-09-18T11:36:11Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43S30 SPIFI1 Bug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837923#M33392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SPIFI.1 errata applies only for below devices:&lt;/P&gt;&lt;P&gt;LPC4370FET100; LPC4370FET256; LPC4350FET256; LPC4350FET180; LPC4330FET256; LPC4330FET180; LPC4330FET100; LPC4330FBD144; LPC4320FET100; LPC4320FBD144; LPC4310FET100; LPC4310FBD144; Cortex-M4 flashless; Rev A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No for the LPC43S30 Revision D device.&lt;/P&gt;&lt;P&gt;Which flash are you using?&lt;/P&gt;&lt;P&gt;Could you please try the suggestions from next links:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/420593"&gt;SPIFI boot issue&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/420486"&gt;SPIFI Errata and Part Version Information&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Sep 2018 15:14:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837923#M33392</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-09-20T15:14:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43S30 SPIFI1 Bug</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837924#M33393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we are using S25FL132K flash. However, I don't&amp;nbsp;see how the flash type could possibly make a difference as not a single clock pulse is output by the LPC SPIFI?&lt;/P&gt;&lt;P&gt;Our problem seems to differ from those treated in both suggested links.&lt;/P&gt;&lt;P&gt;In&amp;nbsp;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/420724"&gt;https://community.nxp.com/thread/420724&lt;/A&gt;&amp;nbsp;LPCware posts:&lt;/P&gt;&lt;P lang="zxx" style="margin-bottom: 0cm;"&gt;&lt;/P&gt;&lt;P lang="zxx" style="margin-bottom: 0cm;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;"One reason for a cold boot fail is of course the SPIFI problem mentioned in the error sheet, where it fails with the first reset but works with the second reset. At power-up it works in the first step. It also works with one reset and then wait for 60 seconds, then the bootloader runs into a timeout and initiates a core reset (= second reset)."&lt;/SPAN&gt;&lt;/P&gt;&lt;P lang="zxx" style="margin-bottom: 0cm;"&gt;&lt;/P&gt;&lt;P lang="zxx" style="margin-bottom: 0cm;"&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;This seems to be exactly our problem but on a 4330, not on a 43S30 revision D device?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Tobias&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Sep 2018 13:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43S30-SPIFI1-Bug/m-p/837924#M33393</guid>
      <dc:creator>tobiasmeyer</dc:creator>
      <dc:date>2018-09-21T13:53:35Z</dc:date>
    </item>
  </channel>
</rss>