<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Lpc1517 build setting in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc1517-build-setting/m-p/837157#M33369</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on LPC1517.&lt;/P&gt;&lt;P&gt;I am using uvision5.&lt;/P&gt;&lt;P&gt;I builded my program code and i got my hex file without error.&lt;/P&gt;&lt;P&gt;But when i programmed my lpc1517 with this version,&amp;nbsp; it does not start!!!&lt;/P&gt;&lt;P&gt;If i remove one line code ex: i++; and i rebuild it .. it is working!!! But i need to add some functions but i can't!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It likes i reached a limit but my flash has 256KB and my code takes only 60KB.&lt;/P&gt;&lt;P&gt;I had enough space of ram too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65977iE24CDDE46A1B4822/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65978iF2FFCF9CDF15D92B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And i can use only Level 0 (the program is not working if i use the other other level??)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is my problem?? (i attached my map file just in case)&lt;/P&gt;&lt;P&gt;Thx for your response&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Jul 2018 12:28:41 GMT</pubDate>
    <dc:creator>martin_pelletie</dc:creator>
    <dc:date>2018-07-20T12:28:41Z</dc:date>
    <item>
      <title>Lpc1517 build setting</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc1517-build-setting/m-p/837157#M33369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working on LPC1517.&lt;/P&gt;&lt;P&gt;I am using uvision5.&lt;/P&gt;&lt;P&gt;I builded my program code and i got my hex file without error.&lt;/P&gt;&lt;P&gt;But when i programmed my lpc1517 with this version,&amp;nbsp; it does not start!!!&lt;/P&gt;&lt;P&gt;If i remove one line code ex: i++; and i rebuild it .. it is working!!! But i need to add some functions but i can't!!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It likes i reached a limit but my flash has 256KB and my code takes only 60KB.&lt;/P&gt;&lt;P&gt;I had enough space of ram too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65977iE24CDDE46A1B4822/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_4.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65978iF2FFCF9CDF15D92B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;And i can use only Level 0 (the program is not working if i use the other other level??)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is my problem?? (i attached my map file just in case)&lt;/P&gt;&lt;P&gt;Thx for your response&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;:smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 12:28:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc1517-build-setting/m-p/837157#M33369</guid>
      <dc:creator>martin_pelletie</dc:creator>
      <dc:date>2018-07-20T12:28:41Z</dc:date>
    </item>
    <item>
      <title>Re: Lpc1517 build setting</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc1517-build-setting/m-p/837158#M33370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have uvision5 evaluation version?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Keil development development tools without a current product license run as a Lite/Evaluation edition and have the following restrictions:&lt;/P&gt;&lt;H5&gt;MDK-ARM Lite Edition&lt;/H5&gt;&lt;UL&gt;&lt;LI&gt;Programs that generate more than 32 Kbytes of code and data will not compile, assemble, or link.&lt;/LI&gt;&lt;LI&gt;The debugger supports programs that are 32 Kbytes or smaller.&lt;/LI&gt;&lt;LI&gt;The compiler does not generate a disassembly listing of the machine code generated. The -S, --asm, and --interleave compiler command-line options are disabled. Projects will not compile with Target -&amp;gt; Listing -&amp;gt; C Compiler Listing enabled.&lt;/LI&gt;&lt;LI&gt;The compiler and assembler do not generate position-independent code or data. The --apcs /ropi /rwpi /pic/ pid compiler and assembler command line options are disabled.&lt;/LI&gt;&lt;LI&gt;The assembler and linker create Symbolic Output Format objects which cannot be linked with third-party linker utilities. Fully licensed tools generate standard ELF/DWARF files which may be used with third-party utilities.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Jul 2018 17:20:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Lpc1517-build-setting/m-p/837158#M33370</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2018-07-24T17:20:46Z</dc:date>
    </item>
  </channel>
</rss>