<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMCUExpresso and ea LPC1788 tcpecho sample</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUExpresso-and-ea-LPC1788-tcpecho-sample/m-p/837115#M33367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering is anybody has experienced problems trying to debug the sample tcpecho_freertos sample. I have successfully imported the project and the necessary board and chip&amp;nbsp; support into an MCUExpresso Workspace. I can build and download it to the Embedded Artists LPC1788 dev but I cannot run debug it without crashing at the network interface initialization (netinf).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I reset the board after the crash I can see the example running. At this point, I can ping the address I assigned it and I can&amp;nbsp; attach the debugger. Any points here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vladimir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Nov 2018 21:33:33 GMT</pubDate>
    <dc:creator>vbravosalazar</dc:creator>
    <dc:date>2018-11-14T21:33:33Z</dc:date>
    <item>
      <title>MCUExpresso and ea LPC1788 tcpecho sample</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUExpresso-and-ea-LPC1788-tcpecho-sample/m-p/837115#M33367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering is anybody has experienced problems trying to debug the sample tcpecho_freertos sample. I have successfully imported the project and the necessary board and chip&amp;nbsp; support into an MCUExpresso Workspace. I can build and download it to the Embedded Artists LPC1788 dev but I cannot run debug it without crashing at the network interface initialization (netinf).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, if I reset the board after the crash I can see the example running. At this point, I can ping the address I assigned it and I can&amp;nbsp; attach the debugger. Any points here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vladimir&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Nov 2018 21:33:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUExpresso-and-ea-LPC1788-tcpecho-sample/m-p/837115#M33367</guid>
      <dc:creator>vbravosalazar</dc:creator>
      <dc:date>2018-11-14T21:33:33Z</dc:date>
    </item>
    <item>
      <title>Re: MCUExpresso and ea LPC1788 tcpecho sample</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCUExpresso-and-ea-LPC1788-tcpecho-sample/m-p/837116#M33368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which MCUXpresso IDE version do you have?&lt;/P&gt;&lt;P&gt;Which OS do you have?&amp;nbsp;&lt;/P&gt;&lt;P&gt;does it happen with the other LPCOpen examples?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please try to create a new workspace and import your projects into the new workspace.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Feb 2019 14:03:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCUExpresso-and-ea-LPC1788-tcpecho-sample/m-p/837116#M33368</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-02-05T14:03:07Z</dc:date>
    </item>
  </channel>
</rss>